PreviousLocation
Syntax
<MU-Path>.PreviousLocation → object |
The read-only attribute PreviousLocation returns the previous location of the MU designated by <MU-Path>. The previous location is the object on which the part was located before it moved onto the current material flow object.
Return Value
The attribute returns a value of data type object.
Example
print .MUs.Part:22037.PreviousLocation |