RemainingProcTime
Syntax
<MU-Path>.RemainingProcTime → time |
The read-only attribute RemainingProcTime returns the time which the MU designated by <MU-Path> still has to be processed.
Return Value
The return value has the data type time.
You can also view the remaining processing time in the dialog Show Attributes and Methods of the object.
Example
print .MUs.Part:872564.RemainingProcTime |