Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.tooling |
Provides classes and interfaces for Tooling.
|
nxopen.userdefinedobjects |
Provides classes and interfaces for User Defined Objects (UDOs).
|
Modifier and Type | Method and Description |
---|---|
UserDefinedObject |
UserDefinedObjectFeatureBuilder.userDefinedObject()
Returns the associated UserDefinedObject
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
UserDefinedObjectFeatureBuilder.setUserDefinedObject(UserDefinedObject userDefinedObject)
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
ColorExpressionsBuilder.setCurrentUDO(UserDefinedObject udo)
Select current udo
License requirements: ug_mold_design ("UG MOLD") OR prog_die_wizard ("UG/Progressive Die Wizard") . |
Modifier and Type | Field and Description |
---|---|
UserDefinedObject |
UserDefinedObjectManager.LinkedUdoDefinition.associatedUdo |
Modifier and Type | Method and Description |
---|---|
UserDefinedObject |
UserDefinedObjectManager.createUserDefinedObject(UserDefinedClass udoClass)
Constructs a new
UserDefinedObjectFeature . |
UserDefinedObject |
UserDefinedObjectManager.getOwningUserDefinedObject(TaggedObject linkObject)
Queries an NX Object to find the
UserDefinedObject that owns the given NXObject (note this will return null for the owning udo if the object is not owned)
License requirements: None. |
UserDefinedObject[] |
UserDefinedObjectManager.getUdosOfClass(UserDefinedClass udoClass)
Finds all
UserDefinedObject instances that use the given UserDefinedClass . |
UserDefinedObject |
UserDefinedEvent.userDefinedObject()
Returns the related UDO.
|
Constructor and Description |
---|
LinkedUdoDefinition(UserDefinedObject.LinkType linkTypeInitial,
UserDefinedObject associatedUdoInitial,
UserDefinedObject.LinkStatus statusInitial)
Constructor for the LinkedUdoDefinition object.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.