public static class UserDefinedObject.LinkType extends Enum
UserDefinedObjectFeature
.Modifier and Type | Field and Description |
---|---|
static int |
_OWNING
The object is owned by the UDO
|
static int |
_TYPE1
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
static int |
_TYPE2
If the UDO is deleted the link between the UDO and the associated object is removed and the object is deleted.
|
static int |
_TYPE3
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
static int |
_TYPE4
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
static UserDefinedObject.LinkType |
OWNING
The object is owned by the UDO
|
static UserDefinedObject.LinkType |
TYPE1
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
static UserDefinedObject.LinkType |
TYPE2
If the UDO is deleted the link between the UDO and the associated object is removed and the object is deleted.
|
static UserDefinedObject.LinkType |
TYPE3
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
static UserDefinedObject.LinkType |
TYPE4
If the UDO is deleted the link between the UDO and the associated object is removed and the object is unaffected.
|
Modifier and Type | Method and Description |
---|---|
static UserDefinedObject.LinkType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static UserDefinedObject.LinkType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static UserDefinedObject.LinkType[] |
values()
Returns an array that contains the values for this enum.
|
public static final UserDefinedObject.LinkType OWNING
public static final UserDefinedObject.LinkType TYPE1
public static final UserDefinedObject.LinkType TYPE2
public static final UserDefinedObject.LinkType TYPE3
public static final UserDefinedObject.LinkType TYPE4
public static final int _OWNING
public static final int _TYPE1
public static final int _TYPE2
public static final int _TYPE3
public static final int _TYPE4
public static UserDefinedObject.LinkType valueOf(int value)
public static UserDefinedObject.LinkType valueOf(String name)
public static UserDefinedObject.LinkType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.