public interface Line extends DisplayableObject
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
INXObject |
findObject(String journalIdentifier)
Finds the
ProcessSetup with the given identifier as recorded in a journal. |
ProcessPlan |
getProcessPlan()
Get the Process plan
License requirements: None. |
ProcessSetup[] |
getSetups()
Get the Setups
License requirements: None. |
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
ProcessPlan getProcessPlan() throws NXException, RemoteException
NXException
RemoteException
ProcessSetup[] getSetups() throws NXException, RemoteException
NXException
RemoteException
INXObject findObject(String journalIdentifier) throws NXException, RemoteException
ProcessSetup
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
findObject
in interface INXObject
journalIdentifier
- Name of the setup to be foundNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.