public interface ProcessPlan extends DisplayableObject
MachiningLinePlanner
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
INXObject |
findObject(String journalIdentifier)
Finds the
Line , not allocated ProcessSetup or Product
with the given identifier as recorded in a journal. |
Line |
getLine()
Get the Line
License requirements: None. |
ProcessSetup |
getNotAllocatedSetup()
Get the Not Allocated setup
License requirements: None. |
Product[] |
getProducts()
Get the Products being manufactured in this ProcessPlan
License requirements: None. |
ProcessSetup[] |
getSetups()
Get the Setups of this ProcessPlan in the order in which they are machined
License requirements: None. |
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
ProcessSetup getNotAllocatedSetup() throws NXException, RemoteException
NXException
RemoteException
Line getLine() throws NXException, RemoteException
NXException
RemoteException
Product[] getProducts() throws NXException, RemoteException
NXException
RemoteException
ProcessSetup[] getSetups() throws NXException, RemoteException
NXException
RemoteException
INXObject findObject(String journalIdentifier) throws NXException, RemoteException
Line
, not allocated ProcessSetup
or Product
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
findObject
in interface INXObject
journalIdentifier
- Name of the line, not allocated setup or product to be foundNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.