Interface | Description |
---|---|
Blank |
Represents a Machining Line Planner blank
To obtain an instance of this class use GetBlankModel of Product. |
InProcessFeature |
Represents a Machining Line Planner in-process feature
To obtain an instance of this class use GetInProcessFeatures of Operation or MachiningFeature. |
IProcess |
Interface to the Machining Line Planner process
This is an abstract class, and cannot be instantiated. |
IResource |
Interface to the Machining Line Planner resource
This is an abstract class, and cannot be instantiated. |
Line |
Represents a Machining Line Planner line
To obtain an instance of this class use GetLine of ProcessPlan or ProcessSetup. |
MachineTool |
Represents a Machining Line Planner machine tool
To obtain an instance of this class use GetMachineTool (not yet implemented!) |
MachiningFeature |
Represents a Machining Line Planner machining feature
To obtain an instance of this class use GetMachiningFeature of InProcessFeature or GetMachiningFeatures of Workpiece or PartFeature. |
MachiningLinePlanner |
Represents the Line Planner
Use the static method in this class to obtain an instance. |
Operation |
Represents a Machining Line Planner operation
To obtain an instance of this class use GetOperation of InProcessFeature or GetOperations of ProcessSetup. |
Part |
Represents a Machining Line Planner part
To obtain an instance of this class use GetPartModel of Product or PartFeature. |
PartFeature |
Represents a Machining Line Planner part-feature
To obtain an instance of this class use GetPartFeature of MachiningFeature or GetPartFeatures or Part. |
ProcessPlan |
Represents a Machining Line Planner process plan
To obtain an instance of this class use MachiningLinePlanner Created in NX11.0.1 |
ProcessSetup |
Represents a Machining Line Planner process setup
To obtain an instance of this class use GetSetup of Operation, Workpiece or ToolSet or GetSetups on ProcessPlan or Line. |
Product |
Represents a Machining Line Planner product
To obtain an instance of this class use GetProducts of ProcessPlan. |
ToolAssembly |
Represents a Machining Line Planner tool assembly
To obtain an instance of this class use (not yet implemented!) |
ToolSet |
Represents a Machining Line Planner tool set
To obtain an instance of this class use GetToolSet of ToolAssembly. |
Workpiece |
Represents a Machining Line Planner workpiece
To obtain an instance of this class, use GetWorkpiece of MachiningFeature or GetWorkpieces of ProcessSetup or Product. |
Class | Description |
---|---|
MachiningLinePlannerFactory |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.