public interface ProcessSetup extends DisplayableObject, IProcess
DisplayableObject.ObjectFont, DisplayableObject.ObjectWidth
NXObject.AttributeInformation, NXObject.AttributeType, NXObject.ComputationalTime, NXObject.DateAndTimeFormat, NXObject.NextUserAttributeData
Modifier and Type | Method and Description |
---|---|
INXObject |
findObject(String journalIdentifier)
Finds the
Operation , Workpiece ,
ToolSet or MachineTool
with the given identifier as recorded in a journal. |
Line |
getLine()
Get the Line of this setup
License requirements: None. |
Operation[] |
getOperations()
Get the Operations in this Setup in the order in which they are machined
License requirements: None. |
ProcessPlan |
getProcessPlan()
Get the Process plan of this setup
License requirements: None. |
ToolSet |
getToolSet()
Get the Tool Set
License requirements: None. |
Workpiece[] |
getWorkpieces()
Get the Workpieces being manufactured in this setup
License requirements: None. |
boolean |
isNotAllocated()
Is this setup the Not Allocated setup
License requirements: None. |
blank, color, highlight, isBlanked, layer, lineFont, lineWidth, nameLocation, redisplayObject, removeViewDependency, setColor, setLayer, setLineFont, setLineWidth, setNameLocation, unblank, unhighlight
createAttributeIterator, deleteAllAttributesByType, deleteAllAttributesByType, deleteAttributeByTypeAndTitle, deleteAttributeByTypeAndTitle, deleteUserAttribute, deleteUserAttributes, deleteUserAttributes, getAttributeTitlesByType, getBooleanUserAttribute, getComputationalTimeUserAttribute, getIntegerAttribute, getIntegerUserAttribute, getNextUserAttribute, getPdmReferenceAttributeValue, getRealAttribute, getRealUserAttribute, getReferenceAttribute, getStringAttribute, getStringUserAttribute, getTimeAttribute, getTimeUserAttribute, getUserAttribute, getUserAttribute, getUserAttributeAsString, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeCount, getUserAttributeLock, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributes, getUserAttributesAsStrings, getUserAttributeSize, getUserAttributeSourceObjects, hasUserAttribute, hasUserAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setAttribute, setBooleanUserAttribute, setPdmReferenceAttribute, setReferenceAttribute, setReferenceAttribute, setTimeAttribute, setTimeAttribute, setTimeUserAttribute, setTimeUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttribute, setUserAttributeLock
printTestData, printTestData, tag, tagValue
isOccurrence, journalIdentifier, name, owningComponent, owningPart, print, prototype, setName
getConstraintPredecessors, getConstraintSuccessors, getPredecessors, getResource, getSuccessors
ProcessPlan getProcessPlan() throws NXException, RemoteException
NXException
RemoteException
boolean isNotAllocated() throws NXException, RemoteException
NXException
RemoteException
Line getLine() throws NXException, RemoteException
NXException
RemoteException
Workpiece[] getWorkpieces() throws NXException, RemoteException
NXException
RemoteException
Operation[] getOperations() throws NXException, RemoteException
NXException
RemoteException
ToolSet getToolSet() throws NXException, RemoteException
NXException
RemoteException
INXObject findObject(String journalIdentifier) throws NXException, RemoteException
Operation
, Workpiece
,
ToolSet
or MachineTool
with the given identifier as recorded in a journal.
An object may not return the same value as its JournalIdentifier in different versions of
the software. However newer versions of the software should find the same object when
FindObject is passed older versions of its journal identifier. In general, this method
should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
findObject
in interface INXObject
journalIdentifier
- Name of the operation, workpiece, machinetool or toolset to be foundNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.