Package | Description |
---|---|
nxopen.features |
Provides classes and interfaces for features.
|
nxopen.features.shipdesign |
Provides classes and interfaces for Ship Design.
|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
ProjectionOptions |
CombinedProjectionBuilder.direction1()
Returns the combined projection direction1
License requirements: None. |
ProjectionOptions |
CombinedProjectionBuilder.direction2()
Returns the combined projection direction2
License requirements: None. |
ProjectionOptions |
ReplaceFaceBuilder.freeEdgeProjection()
Returns the free edge projection options, which defines a direction to project laminar boundaries of the original face onto the replacement face.
|
ProjectionOptions |
SnipSurfaceBuilder.projectDirection()
Returns the project direction
License requirements: solid_modeling ("SOLIDS MODELING") OR studio_free_form ("STUDIO FREE FORM") . |
ProjectionOptions |
GeodesicProjectBuilder.projectDirection()
Returns the project direction of point
License requirements: None. |
ProjectionOptions |
AeroRibBuilder.projectDirection()
Returns the project direction
License requirements: None. |
ProjectionOptions |
AeroFlangeBuilder.projectDirection()
Returns the project direction
License requirements: None. |
ProjectionOptions |
ShelfBuilder.projectionDir1()
Returns the project direction 1
License requirements: None. |
ProjectionOptions |
ShelfBuilder.projectionDir2()
Returns the project direction 2
License requirements: None. |
ProjectionOptions |
VarOffsetFaceBuilder.projectionDirection()
Returns the projection direction
License requirements: None. |
ProjectionOptions |
TrimSheetBuilder.projectionDirection()
Returns the projection direction
License requirements: None. |
ProjectionOptions |
HolePackageBuilder.projectionDirection()
Returns the hole direction options
License requirements: None. |
ProjectionOptions |
StepBuilder.projectionDirection1()
Returns the project direction options used to project boundary section curve 1 onto the belt face
License requirements: None. |
ProjectionOptions |
StepBuilder.projectionDirection2()
Returns the project direction options used to project boundary section curve 2 onto the belt face
License requirements: None. |
ProjectionOptions |
DividefaceBuilder.projectionOption()
Returns the Projection Options data
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ProjectionOptions |
SeamBuilder.definitionProjectionDirection()
Returns the direction to project curves to the ship structure to define seams.
|
ProjectionOptions |
PlateBuilder.projectDirection()
Returns the project direction, which is used to project the boundary curves to the plate mold face.
|
ProjectionOptions |
StiffenerSystemBuilder.projectionDirection()
Returns the direction used to project the stiffener path object
License requirements: None. |
ProjectionOptions |
PlateSystemBuilder.projectionDirection()
Returns the direction used to project
the boundary section curves onto the mold face.
|
ProjectionOptions |
Cutout2Builder.projectionDirection()
Returns the direction used to project the custom shape curves
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
ProjectionOptions |
SurfaceWeldBuilder.projectionDirection()
Returns the project direction, which is used to project the boundary curves to the plate mold face.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.