public interface GeodesicProjectBuilder extends FeatureBuilder
GeodesicProject
builder for Project command. GeodesicSketchCollection.createGeodesicProjectBuilder(nxopen.features.GeodesicProject)
Property | Value |
---|---|
ProjectType | Curve |
Modifier and Type | Interface and Description |
---|---|
static class |
GeodesicProjectBuilder.Type
Represents the type of objects projected to the support faces.
|
Modifier and Type | Method and Description |
---|---|
Section |
projectCurves()
Returns the curves to project
License requirements: None. |
ProjectionOptions |
projectDirection()
Returns the project direction of point
License requirements: None. |
Point |
projectPoint()
Returns the point to project
License requirements: None. |
GeodesicProjectBuilder.Type |
projectType()
Returns the project
License requirements: None. |
void |
setProjectPoint(Point projectPoint)
License requirements: solid_modeling ("SOLIDS MODELING") . |
void |
setProjectType(GeodesicProjectBuilder.Type projectType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
commitFeature, getFeature, hideInternalParentFeatureAfterEdit, parentFeatureInternal, patchSolutionFlag, patchSurfaceFilename, setParentFeatureInternal, setParentFeatureInternal, setPatchSolutionFlag, setPatchSurfaceFilename, setSurroundingPatchSurfaceFilename, showInternalParentFeatureForEdit, surroundingPatchSurfaceFilename, unsetParentFeatureInternal
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
GeodesicProjectBuilder.Type projectType() throws NXException, RemoteException
NXException
RemoteException
void setProjectType(GeodesicProjectBuilder.Type projectType) throws NXException, RemoteException
projectType
- NXException
RemoteException
Section projectCurves() throws NXException, RemoteException
NXException
RemoteException
Point projectPoint() throws NXException, RemoteException
NXException
RemoteException
void setProjectPoint(Point projectPoint) throws NXException, RemoteException
projectPoint
- NXException
RemoteException
ProjectionOptions projectDirection() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.