See: Description
Interface | Description |
---|---|
FaceAnnotationBuilder |
Builder for Face Annotation functionality used in formboard.
|
FlipComponentBuilder |
Builder for flip component operation used in formboard.
|
FormboardLayoutBuilder |
Class that performs the "layout" of Formboard geometry.
|
FormboardManager |
Contains information about flattened harness drawing and drafting data for
harness manufacturing drawings (Formboard Drawings).
|
LayoutLengthOptions |
Defines the various options for determining the rounded lengths of
formboard geometry during the layout or update process.
|
ObjectAttributeReferenceBuilder |
Builder for "object attribute" used in formboard which enbles user to create
annotation in drafting functionality.
|
OrientBranchBuilder |
Builder for "Orient Branch" operation used in formboard.
|
PathLengthAnnotationBuilder |
TODO Class documentation
To create a new instance of this class, use FormboardManager.createPathLengthAnnotationBuilder(nxopen.annotations.Annotation) Default values. |
ShapeSegmentBuilder |
Builder for Face Annotation functionality used in formboard.
|
UpdateDiscrepancy |
Defines a discrepancy object which contains information about a specific
difference between the formboard drawing and the 3D harness model.
|
UpdateFormboardBuilder |
Class that performs the "update" of Formboard geometry.
|
Class | Description |
---|---|
FaceAnnotationBuilder.DrwDestination |
Enum which defines where the geometry is to be placed.
|
FaceAnnotationBuilder.Types |
Enum which defines the type to import CGM/Pattern file
|
FlipComponentBuilder.AxisType |
Enum for the selection of axis type for flipping formboard component
|
FormboardLayoutBuilder.BranchAngle |
Methods for determining which angles to apply at each branch of the Formboard.
|
FormboardLayoutBuilder.BranchShape |
Shape option for the branches.
|
FormboardLayoutBuilder.MainRunType |
Selection method for the set of segments that define the main
run of the formboard geometry.
|
LayoutLengthOptions.RoundingMethod |
Methods of rounding lengths for Formboard geometry.
|
ObjectAttributeReferenceBuilder.LeaderType |
Enum which defines types of leader user wants to associate with the annotation.
|
OrientBranchBuilder.BranchAngleMethod |
Enum to define the type of method to orient branch.
|
PathLengthAnnotationBuilder.Types |
TODO: Document the whole type
|
ShapeSegmentBuilder.LineData |
This class holds the data returned from
ShapeSegmentBuilder.getLineData() |
UpdateDiscrepancy.ObjectType |
Specifies the type of objects involved in the discrepancy.
|
UpdateDiscrepancy.Type |
The general type of the discrepancy.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.