public static class OrientBranchBuilder.BranchAngleMethod extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALIGN_AXIS_TO_VECTOR
method to rotate branch by an angle between two vectors
|
static int |
_ANGLE
method to rotate branch by angle
|
static int |
_ANGLEFROM_REFERENCE_VECTOR
method to rotate branch with respect to selected vectors
|
static int |
_TWO_POINTS
method to rotate branch by and angle between two points
|
static OrientBranchBuilder.BranchAngleMethod |
ALIGN_AXIS_TO_VECTOR
method to rotate branch by an angle between two vectors
|
static OrientBranchBuilder.BranchAngleMethod |
ANGLE
method to rotate branch by angle
|
static OrientBranchBuilder.BranchAngleMethod |
ANGLEFROM_REFERENCE_VECTOR
method to rotate branch with respect to selected vectors
|
static OrientBranchBuilder.BranchAngleMethod |
TWO_POINTS
method to rotate branch by and angle between two points
|
Modifier and Type | Method and Description |
---|---|
static OrientBranchBuilder.BranchAngleMethod |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static OrientBranchBuilder.BranchAngleMethod |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static OrientBranchBuilder.BranchAngleMethod[] |
values()
Returns an array that contains the values for this enum.
|
public static final OrientBranchBuilder.BranchAngleMethod ANGLEFROM_REFERENCE_VECTOR
public static final OrientBranchBuilder.BranchAngleMethod ANGLE
public static final OrientBranchBuilder.BranchAngleMethod ALIGN_AXIS_TO_VECTOR
public static final OrientBranchBuilder.BranchAngleMethod TWO_POINTS
public static final int _ANGLEFROM_REFERENCE_VECTOR
public static final int _ANGLE
public static final int _ALIGN_AXIS_TO_VECTOR
public static final int _TWO_POINTS
public static OrientBranchBuilder.BranchAngleMethod valueOf(int value)
public static OrientBranchBuilder.BranchAngleMethod valueOf(String name)
public static OrientBranchBuilder.BranchAngleMethod[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.