public static class ObjectAttributeReferenceBuilder.LeaderType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_NONE
No leader for annotation of selected object.
|
static int |
_SINGLE_LOCATION
Single leader for the annotation of selected object.
|
static int |
_STARTAND_END_LOCATIONS
Two leaders for annotation with start and end location.
|
static ObjectAttributeReferenceBuilder.LeaderType |
NONE
No leader for annotation of selected object.
|
static ObjectAttributeReferenceBuilder.LeaderType |
SINGLE_LOCATION
Single leader for the annotation of selected object.
|
static ObjectAttributeReferenceBuilder.LeaderType |
STARTAND_END_LOCATIONS
Two leaders for annotation with start and end location.
|
Modifier and Type | Method and Description |
---|---|
static ObjectAttributeReferenceBuilder.LeaderType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ObjectAttributeReferenceBuilder.LeaderType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ObjectAttributeReferenceBuilder.LeaderType[] |
values()
Returns an array that contains the values for this enum.
|
public static final ObjectAttributeReferenceBuilder.LeaderType NONE
public static final ObjectAttributeReferenceBuilder.LeaderType SINGLE_LOCATION
public static final ObjectAttributeReferenceBuilder.LeaderType STARTAND_END_LOCATIONS
public static final int _NONE
public static final int _SINGLE_LOCATION
public static final int _STARTAND_END_LOCATIONS
public static ObjectAttributeReferenceBuilder.LeaderType valueOf(int value)
public static ObjectAttributeReferenceBuilder.LeaderType valueOf(String name)
public static ObjectAttributeReferenceBuilder.LeaderType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.