public static class NonProportionalZoom.MethodType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_DYNAMIC
Defines a line to define aspect ratio of non-proportional zoom.
|
static int |
_RECTANGLE
Uses a rectangular region to be zoomed.
|
static NonProportionalZoom.MethodType |
DYNAMIC
Defines a line to define aspect ratio of non-proportional zoom.
|
static NonProportionalZoom.MethodType |
RECTANGLE
Uses a rectangular region to be zoomed.
|
Modifier and Type | Method and Description |
---|---|
static NonProportionalZoom.MethodType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NonProportionalZoom.MethodType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NonProportionalZoom.MethodType[] |
values()
Returns an array that contains the values for this enum.
|
public static final NonProportionalZoom.MethodType RECTANGLE
public static final NonProportionalZoom.MethodType DYNAMIC
public static final int _RECTANGLE
public static final int _DYNAMIC
public static NonProportionalZoom.MethodType valueOf(int value)
public static NonProportionalZoom.MethodType valueOf(String name)
public static NonProportionalZoom.MethodType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.