public interface PerspectiveOptionsBuilder extends Builder
Modifier and Type | Method and Description |
---|---|
void |
applyLastDistanceChange()
Sets the work view to have the camera distance, which is the distance from the camera's
position to the target position in the work view which was specified in the last use of
setCameraDistance(double)
The camera distance has no meaning for an orthographic view, so this method does nothing
if the work view is an orthographic view. |
double |
cameraDistance()
Returns the camera distance: The distance from the camera's position to the
target position in the work view view when it is a perspective view.
|
void |
cancel()
Cancels the Perspective Options Builder.
|
void |
setCameraDistance(double cameraDistance)
License requirements: None. |
commit, destroy, getCommittedObjects, getObject, showResults
printTestData, printTestData, tag, tagValue
validate
double cameraDistance() throws NXException, RemoteException
NXException
RemoteException
void setCameraDistance(double cameraDistance) throws NXException, RemoteException
cameraDistance
- NXException
RemoteException
void applyLastDistanceChange() throws NXException, RemoteException
setCameraDistance(double)
The camera distance has no meaning for an orthographic view, so this method does nothing
if the work view is an orthographic view.
NXException
RemoteException
void cancel() throws NXException, RemoteException
NXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.