Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static NonProportionalZoom.MethodType |
NonProportionalZoom.MethodType.DYNAMIC
Defines a line to define aspect ratio of non-proportional zoom.
|
static NonProportionalZoom.MethodType |
NonProportionalZoom.MethodType.RECTANGLE
Uses a rectangular region to be zoomed.
|
Modifier and Type | Method and Description |
---|---|
NonProportionalZoom.MethodType |
NonProportionalZoom.method()
Returns the type of mouse interaction used to define the non-proportional zoom.
|
static NonProportionalZoom.MethodType |
NonProportionalZoom.MethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static NonProportionalZoom.MethodType |
NonProportionalZoom.MethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static NonProportionalZoom.MethodType[] |
NonProportionalZoom.MethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
NonProportionalZoom.setMethod(NonProportionalZoom.MethodType method)
License requirements: studio_analyze ("STUDIO ANALYZE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.