public static class DecalBuilder.DecalIllumination extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_USE_DECAL_MATERIAL
set decal's reflectivity
|
static int |
_USE_UNDERLYING_MATERIAL
base decal reflectivity on underlying material
|
static DecalBuilder.DecalIllumination |
USE_DECAL_MATERIAL
set decal's reflectivity
|
static DecalBuilder.DecalIllumination |
USE_UNDERLYING_MATERIAL
base decal reflectivity on underlying material
|
Modifier and Type | Method and Description |
---|---|
static DecalBuilder.DecalIllumination |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecalBuilder.DecalIllumination |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecalBuilder.DecalIllumination[] |
values()
Returns an array that contains the values for this enum.
|
public static final DecalBuilder.DecalIllumination USE_UNDERLYING_MATERIAL
public static final DecalBuilder.DecalIllumination USE_DECAL_MATERIAL
public static final int _USE_UNDERLYING_MATERIAL
public static final int _USE_DECAL_MATERIAL
public static DecalBuilder.DecalIllumination valueOf(int value)
public static DecalBuilder.DecalIllumination valueOf(String name)
public static DecalBuilder.DecalIllumination[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.