Package | Description |
---|---|
nxopen.display |
Provides classes and interfaces for Display.
|
Modifier and Type | Field and Description |
---|---|
static DecalBuilder.DecalIllumination |
DecalBuilder.DecalIllumination.USE_DECAL_MATERIAL
set decal's reflectivity
|
static DecalBuilder.DecalIllumination |
DecalBuilder.DecalIllumination.USE_UNDERLYING_MATERIAL
base decal reflectivity on underlying material
|
Modifier and Type | Method and Description |
---|---|
DecalBuilder.DecalIllumination |
DecalBuilder.illuminationType()
Returns the illumination type
License requirements: None. |
static DecalBuilder.DecalIllumination |
DecalBuilder.DecalIllumination.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecalBuilder.DecalIllumination |
DecalBuilder.DecalIllumination.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecalBuilder.DecalIllumination[] |
DecalBuilder.DecalIllumination.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DecalBuilder.setIlluminationType(DecalBuilder.DecalIllumination illuminationType)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.