public static class DecalBuilder.DecalReflectivities extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_USE_GLASS |
static int |
_USE_MATTE |
static int |
_USE_METAL |
static int |
_USE_MIRROR |
static int |
_USE_PLASTIC |
static DecalBuilder.DecalReflectivities |
USE_GLASS |
static DecalBuilder.DecalReflectivities |
USE_MATTE |
static DecalBuilder.DecalReflectivities |
USE_METAL |
static DecalBuilder.DecalReflectivities |
USE_MIRROR |
static DecalBuilder.DecalReflectivities |
USE_PLASTIC |
Modifier and Type | Method and Description |
---|---|
static DecalBuilder.DecalReflectivities |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DecalBuilder.DecalReflectivities |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DecalBuilder.DecalReflectivities[] |
values()
Returns an array that contains the values for this enum.
|
public static final DecalBuilder.DecalReflectivities USE_MATTE
public static final DecalBuilder.DecalReflectivities USE_PLASTIC
public static final DecalBuilder.DecalReflectivities USE_MIRROR
public static final DecalBuilder.DecalReflectivities USE_METAL
public static final DecalBuilder.DecalReflectivities USE_GLASS
public static final int _USE_MATTE
public static final int _USE_PLASTIC
public static final int _USE_MIRROR
public static final int _USE_METAL
public static final int _USE_GLASS
public static DecalBuilder.DecalReflectivities valueOf(int value)
public static DecalBuilder.DecalReflectivities valueOf(String name)
public static DecalBuilder.DecalReflectivities[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.