Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
nxopen.drawings |
Provides classes and interfaces for Drafting Drawings.
|
nxopen.routing |
Provides classes and interfaces for Routing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Arc
Represents an arc curve.
|
interface |
Axis
Represents an
Axis class. |
interface |
CartesianCoordinateSystem
Represents a cartesian coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCoordinateSystem(nxopen.Point3d, nxopen.Matrix3x3, boolean) Created in NX4.0.0 |
interface |
Conic
Represents a conic curve.
|
interface |
CoordinateSystem
Represents a coordinate system
This is an abstract class . |
interface |
Curve
Represents a curve.
|
interface |
CylindricalCoordinateSystem
Represents a cylindrical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createCylindricalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
Direction
Represents a direction.
|
interface |
Ellipse
Represents an ellipse curve.
|
interface |
Hyperbola
Represents a hyperbola curve.
|
interface |
InfiniteLine
Represents a infinite line curve.
|
interface |
Line
Represents a line curve.
|
interface |
Offset
Represents a
Offset . |
interface |
Parabola
Represents a parabola curve.
|
interface |
Plane
Represents an
Plane class. |
interface |
Point
Represents a smart
Point . |
interface |
Polyline
Represents a polyline curve.
|
interface |
Scalar
Represents a scalar.
|
interface |
SphericalCoordinateSystem
Represents a spherical coordinate system
To create a new instance of this class, use CoordinateSystemCollection.createSphericalCoordinateSystem(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d) Created in NX4.0.0 |
interface |
Spline
Represents a spline curve.
|
interface |
Xform
Represents a smart xform
To create a new instance of this class, use XformCollection.createXform(nxopen.Point3d, nxopen.Vector3d, nxopen.Vector3d, nxopen.SmartObject.UpdateOption, double) Created in NX3.0.0 |
Modifier and Type | Field and Description |
---|---|
SmartObject |
SelectSmartObject.ValueData.selection
selected object
|
SmartObject |
SelectSmartObject.ValueWithCaeSetObjectInfoData.selection
selected object
|
SmartObject |
SelectSmartObject.ValueWithSnapData.selection1
first selected object
|
SmartObject |
SelectSmartObject.ValueWithSnapData.selection2
second selected object
|
Modifier and Type | Method and Description |
---|---|
SmartObject |
SelectSmartObject.value()
Returns the object being selected
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
Sketch.addGeometry(Sketch.InferConstraintsOption inferCoincidentConstraints,
Sketch.AddEllipseOption ellipseOption,
SmartObject[] curvesOrPoints)
Adds an array of curves or points to a sketch.
|
SketchConstraint[] |
Sketch.autoConstrain(double linearTolerance,
double angularTolerance,
boolean allowRemoteConstraints,
SmartObject[] geometries,
Sketch.ConstraintType[] autoconstraintTypes)
Creates Automatic Constraints on input set of geometries.
|
Offset |
OffsetCollection.createCurvature(Point atPoint,
Face face,
Offset.OnFaceOption option,
SmartObject sectionDirection,
SmartObject.UpdateOption updateOption)
|
Offset |
OffsetCollection.createCurvatureDerivative(Point atPoint,
Face face,
Offset.OnFaceOption option,
SmartObject sectionDirection,
SmartObject.UpdateOption updateOption)
|
Direction |
DirectionCollection.createDirection(Point atPoint,
Face face,
Direction.OnFaceOption option,
SmartObject sectionDirection,
Sense sense,
SmartObject.UpdateOption updateOption)
|
SketchConstraint[] |
Sketch.getConstraintsForGeometry(SmartObject geometry,
Sketch.ConstraintClass conClass)
Gets all the constraints associated with a particular geometric item
License requirements: None. |
Sketch |
SketchCollection.getOwningSketch(SmartObject geometry)
Returns the sketch that owns the specified geometry
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
void |
SmartObject.replaceParameters(SmartObject otherSo)
Edit a smart object by replacing its parameters using parameters of
other smart object of the same class.
|
void |
SelectSmartObject.setValue(SmartObject selection)
Sets the object being selected
License requirements: None. |
void |
SelectSmartObject.setValue(SmartObject selection,
View view,
Point3d point)
The object being selected with the object's view and object's point
License requirements: None. |
void |
SelectSmartObject.setValueWithCaeSetObjectInfo(SmartObject selection,
CaeObjectType.CaeSubType caeSubType,
int caeSubId)
Deprecated.
Deprecated in NX10.0.0. Use other versions of
SelectObject.setValue(nxopen.TaggedObject) .
|
void |
SelectSmartObject.setValueWithSnap(InferSnapType.SnapType snapType,
SmartObject selection1,
View view1,
Point3d point1,
SmartObject selection2,
View view2,
Point3d point2)
The object being selected with the objects view and objects point and snap information.
|
void |
Sketch.updateConstraintDisplay(SmartObject[] geoms)
Updates the constraint display of given set of geoms without updating the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Sketch.updateDimensionDisplay(SmartObject[] geoms)
Updates the dimension display of given set of geoms without updating the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
void |
Sketch.updateGeometryDisplay(SmartObject[] geoms)
Updates the geometry display of given set of geoms without updating the sketch
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") OR geometric_tol ("GDT") . |
Modifier and Type | Interface and Description |
---|---|
interface |
MeshPoint
Represents a smart
MeshPoint . |
Modifier and Type | Method and Description |
---|---|
SmartObject |
StrainGageBuilder.csys()
Returns the orientation direction, Only available when the strain gage's orientation plane type is
StrainGageOrientationPlane.CSYS
License requirements: nx_response_anlys ("NX Response Analysis") Created in NX6.0.0 |
Modifier and Type | Method and Description |
---|---|
void |
StrainGageBuilder.setCsys(SmartObject orientationCoordSystem)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Modifier and Type | Method and Description |
---|---|
SmartObject |
NcmTransferBuilder.approachToolAxis()
Returns the approach tool axis
License requirements: None. |
SmartObject |
NcmTransferBuilder.approachVector()
Returns the approach vector
License requirements: None. |
SmartObject |
NcmTransferBuilder.departureToolAxis()
Returns the departure tool axis
License requirements: None. |
SmartObject |
NcmTransferBuilder.departureVector()
Returns the departure vector
License requirements: None. |
SmartObject |
PreprocessGeometryBuilder.fixedVector()
Returns the default tool axis vector
License requirements: cam_base ("CAM BASE") . |
SmartObject |
PmopToolAxisCiBuilder.fixedVector()
Returns the tool axis vector
License requirements: None. |
SmartObject |
RotaryFinishGeomBuilder.partAxisVector()
Returns the part axis vector
License requirements: None. |
SmartObject |
PartAxisBuilder.partAxisVector()
Returns the part axis vector
License requirements: None. |
SmartObject |
MultiBladeGeomBuilder.partAxisVector()
Returns the part axis vector
License requirements: None. |
SmartObject |
NcmPlanarEngRetBuilder.plane()
Returns the engage/retract plane,plane entity type covers Xform and Plane
License requirements: None. |
SmartObject |
NcmScEngRetBuilder.vector()
Returns the engage/retract vector
License requirements: None. |
SmartObject |
NcmPlanarEngRetBuilder.vector()
Returns the engage/retract vector
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
NcmTransferBuilder.setApproachToolAxis(SmartObject newValue)
License requirements: cam_base ("CAM BASE") . |
void |
NcmTransferBuilder.setApproachVector(SmartObject newValue)
License requirements: cam_base ("CAM BASE") . |
void |
NcmTransferBuilder.setDepartureToolAxis(SmartObject newValue)
License requirements: cam_base ("CAM BASE") . |
void |
NcmTransferBuilder.setDepartureVector(SmartObject newValue)
License requirements: cam_base ("CAM BASE") . |
void |
PreprocessGeometryBuilder.setFixedVector(SmartObject newVector)
License requirements: cam_base ("CAM BASE") . |
void |
PmopToolAxisCiBuilder.setFixedVector(SmartObject newValue)
License requirements: cam_base ("CAM BASE") . |
void |
RotaryFinishGeomBuilder.setPartAxisVector(SmartObject vector)
License requirements: cam_base ("CAM BASE") . |
void |
PartAxisBuilder.setPartAxisVector(SmartObject vector)
License requirements: cam_base ("CAM BASE") . |
void |
MultiBladeGeomBuilder.setPartAxisVector(SmartObject vector)
License requirements: cam_base ("CAM BASE") . |
void |
NcmPlanarEngRetBuilder.setPlane(SmartObject plane)
License requirements: cam_base ("CAM BASE") . |
void |
NcmScEngRetBuilder.setVector(SmartObject vector)
License requirements: cam_base ("CAM BASE") . |
void |
NcmPlanarEngRetBuilder.setVector(SmartObject vector)
License requirements: cam_base ("CAM BASE") . |
Modifier and Type | Interface and Description |
---|---|
interface |
DraftingPoint
Represents a Drafting VD Point.
|
Modifier and Type | Interface and Description |
---|---|
interface |
Anchor
A Routing Anchor defines a position in a Qualified Routing component part.
|
interface |
ArcSegment
Represents a arc segment.
|
interface |
ControlPoint
Routing Control Points define a position in space, and are used to determine connections
from segments to segments, and segments to ports.
|
interface |
ExtractPort
Routing ExtractPort object is an extract of Port class
To create an instance of this class use PortCollection.createExtractPort(nxopen.routing.Port) Created in NX4.0.0 |
interface |
FittingPort
Represents a Routing Fitting Port Object
FittingPort . |
interface |
FixturePort
FixturePort objects are objects that
segments are routed through when creating a routing path. |
interface |
GapArcSegment
Represents a gap arc segment.
|
interface |
LineSegment
Represents a line segment.
|
interface |
MultiPort
Represents a
MultiPort . |
interface |
Port
Routing Port Object is a parent class for FixturePort, ExtractPort, FittingPort,
Multiport, StockPort and TerminalPort
Creator not available in KF. |
interface |
ProxyPort
A
ProxyPort is a port that represents a connector in
another design zone, but not present in this design zone. |
interface |
SplineSegment
Represents a spline segment.
|
interface |
StockOffsetPort
StockOffsetPort class handles the relationship
between a component part's port occurrence and the dumb offset port in
the work part. |
interface |
StockPort
|
interface |
TerminalPort
A
TerminalPort models the pins on an electrical
connector. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.