public static class Sketch.ConstraintType extends Enum
Modifier and Type | Method and Description |
---|---|
static Sketch.ConstraintType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.ConstraintType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.ConstraintType[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.ConstraintType NO_CON
public static final Sketch.ConstraintType FIXED
public static final Sketch.ConstraintType HORIZONTAL
public static final Sketch.ConstraintType VERTICAL
public static final Sketch.ConstraintType PARALLEL
public static final Sketch.ConstraintType PERPENDICULAR
public static final Sketch.ConstraintType COLLINEAR
public static final Sketch.ConstraintType EQUAL_LENGTH
public static final Sketch.ConstraintType EQUAL_RADIUS
public static final Sketch.ConstraintType CONSTANT_LENGTH
public static final Sketch.ConstraintType CONSTANT_ANGLE
public static final Sketch.ConstraintType COINCIDENT
public static final Sketch.ConstraintType CONCENTRIC
public static final Sketch.ConstraintType MIRROR
public static final Sketch.ConstraintType POINT_ON_CURVE
public static final Sketch.ConstraintType MIDPOINT
public static final Sketch.ConstraintType TANGENT
public static final Sketch.ConstraintType RADIUS_DIM
public static final Sketch.ConstraintType DIAMETER_DIM
public static final Sketch.ConstraintType HORIZONTAL_DIM
public static final Sketch.ConstraintType VERTICAL_DIM
public static final Sketch.ConstraintType PARALLEL_DIM
public static final Sketch.ConstraintType PERPENDICULAR_DIM
public static final Sketch.ConstraintType ANGULAR_DIM
public static final Sketch.ConstraintType RESERVED_CON1
public static final Sketch.ConstraintType RESERVED_CON2
public static final Sketch.ConstraintType RESERVED_CON3
public static final Sketch.ConstraintType RESERVED_CON4
public static final Sketch.ConstraintType RESERVED_CON5
public static final Sketch.ConstraintType RESERVED_CON6
public static final Sketch.ConstraintType POINT_ON_STRING
public static final Sketch.ConstraintType SLOPE
public static final Sketch.ConstraintType UNIFORM_SCALED
public static final Sketch.ConstraintType NON_UNIFORM_SCALED
public static final Sketch.ConstraintType ASSOC_TRIM
public static final Sketch.ConstraintType ASSOC_OFFSET
public static final Sketch.ConstraintType PERIMETER_DIM
public static final Sketch.ConstraintType OFFSET
public static final Sketch.ConstraintType NORMAL
public static final Sketch.ConstraintType POINT_ON_LOOP
public static final Sketch.ConstraintType RECIPE_TRIM
public static final Sketch.ConstraintType PATTERN
public static final Sketch.ConstraintType MINOR_ANGULAR_DIM
public static final Sketch.ConstraintType MAJOR_ANGULAR_DIM
public static final Sketch.ConstraintType LAST_CON_TYPE
public static final int _NO_CON
public static final int _FIXED
public static final int _HORIZONTAL
public static final int _VERTICAL
public static final int _PARALLEL
public static final int _PERPENDICULAR
public static final int _COLLINEAR
public static final int _EQUAL_LENGTH
public static final int _EQUAL_RADIUS
public static final int _CONSTANT_LENGTH
public static final int _CONSTANT_ANGLE
public static final int _COINCIDENT
public static final int _CONCENTRIC
public static final int _MIRROR
public static final int _POINT_ON_CURVE
public static final int _MIDPOINT
public static final int _TANGENT
public static final int _RADIUS_DIM
public static final int _DIAMETER_DIM
public static final int _HORIZONTAL_DIM
public static final int _VERTICAL_DIM
public static final int _PARALLEL_DIM
public static final int _PERPENDICULAR_DIM
public static final int _ANGULAR_DIM
public static final int _RESERVED_CON1
public static final int _RESERVED_CON2
public static final int _RESERVED_CON3
public static final int _RESERVED_CON4
public static final int _RESERVED_CON5
public static final int _RESERVED_CON6
public static final int _POINT_ON_STRING
public static final int _SLOPE
public static final int _UNIFORM_SCALED
public static final int _NON_UNIFORM_SCALED
public static final int _ASSOC_TRIM
public static final int _ASSOC_OFFSET
public static final int _PERIMETER_DIM
public static final int _OFFSET
public static final int _NORMAL
public static final int _POINT_ON_LOOP
public static final int _RECIPE_TRIM
public static final int _PATTERN
public static final int _MINOR_ANGULAR_DIM
public static final int _MAJOR_ANGULAR_DIM
public static final int _LAST_CON_TYPE
public static Sketch.ConstraintType valueOf(int value)
public static Sketch.ConstraintType valueOf(String name)
public static Sketch.ConstraintType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.