public static class Sketch.ConstraintPointType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ANCHOR
The anchor point of a conic
|
static int |
_ARC_CENTER
Center of a circle, arc, or ellipse
|
static int |
_END_VERTEX
End vertex (e.g. the end point of a line)
|
static int |
_MID_VERTEX
The mid vertex of a line or an arc
|
static int |
_NONE
The geometry is not a point
|
static int |
_SPLINE_DEFINING_POINT
A defining point of a spline.
|
static int |
_SPLINE_POLE
The control pole of a spline
|
static int |
_START_VERTEX
Start vertex (e.g. the start point of a line)
|
static Sketch.ConstraintPointType |
ANCHOR
The anchor point of a conic
|
static Sketch.ConstraintPointType |
ARC_CENTER
Center of a circle, arc, or ellipse
|
static Sketch.ConstraintPointType |
END_VERTEX
End vertex (e.g. the end point of a line)
|
static Sketch.ConstraintPointType |
MID_VERTEX
The mid vertex of a line or an arc
|
static Sketch.ConstraintPointType |
NONE
The geometry is not a point
|
static Sketch.ConstraintPointType |
SPLINE_DEFINING_POINT
A defining point of a spline.
|
static Sketch.ConstraintPointType |
SPLINE_POLE
The control pole of a spline
|
static Sketch.ConstraintPointType |
START_VERTEX
Start vertex (e.g. the start point of a line)
|
Modifier and Type | Method and Description |
---|---|
static Sketch.ConstraintPointType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.ConstraintPointType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.ConstraintPointType[] |
values()
Returns an array that contains the values for this enum.
|
public static final Sketch.ConstraintPointType NONE
public static final Sketch.ConstraintPointType START_VERTEX
public static final Sketch.ConstraintPointType END_VERTEX
public static final Sketch.ConstraintPointType ARC_CENTER
public static final Sketch.ConstraintPointType SPLINE_DEFINING_POINT
public static final Sketch.ConstraintPointType ANCHOR
public static final Sketch.ConstraintPointType SPLINE_POLE
public static final Sketch.ConstraintPointType MID_VERTEX
public static final int _NONE
public static final int _START_VERTEX
public static final int _END_VERTEX
public static final int _ARC_CENTER
public static final int _SPLINE_DEFINING_POINT
public static final int _ANCHOR
public static final int _SPLINE_POLE
public static final int _MID_VERTEX
public static Sketch.ConstraintPointType valueOf(int value)
public static Sketch.ConstraintPointType valueOf(String name)
public static Sketch.ConstraintPointType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.