Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
Modifier and Type | Field and Description |
---|---|
static Sketch.ConstraintType |
Sketch.ConstraintType.ANGULAR_DIM
system will decide if it is major or minor
|
static Sketch.ConstraintType |
Sketch.ConstraintType.ASSOC_OFFSET
Limited support
|
static Sketch.ConstraintType |
Sketch.ConstraintType.ASSOC_TRIM
Limited support
|
static Sketch.ConstraintType |
Sketch.ConstraintType.COINCIDENT |
static Sketch.ConstraintType |
Sketch.ConstraintType.COLLINEAR |
static Sketch.ConstraintType |
Sketch.ConstraintType.CONCENTRIC |
static Sketch.ConstraintType |
Sketch.ConstraintType.CONSTANT_ANGLE |
static Sketch.ConstraintType |
Sketch.ConstraintType.CONSTANT_LENGTH |
static Sketch.ConstraintType |
Sketch.ConstraintType.DIAMETER_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.EQUAL_LENGTH |
static Sketch.ConstraintType |
Sketch.ConstraintType.EQUAL_RADIUS |
static Sketch.ConstraintType |
Sketch.ConstraintType.FIXED |
static Sketch.ConstraintType |
Sketch.ConstraintType.HORIZONTAL |
static Sketch.ConstraintType |
Sketch.ConstraintType.HORIZONTAL_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.LAST_CON_TYPE
The last constraint type indicator;
NOT to be used.
|
static Sketch.ConstraintType |
Sketch.ConstraintType.MAJOR_ANGULAR_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.MIDPOINT |
static Sketch.ConstraintType |
Sketch.ConstraintType.MINOR_ANGULAR_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.MIRROR |
static Sketch.ConstraintType |
Sketch.ConstraintType.NO_CON
Used in query methods that filter by constraint type
to select any type of constraint
|
static Sketch.ConstraintType |
Sketch.ConstraintType.NON_UNIFORM_SCALED |
static Sketch.ConstraintType |
Sketch.ConstraintType.NORMAL |
static Sketch.ConstraintType |
Sketch.ConstraintType.OFFSET |
static Sketch.ConstraintType |
Sketch.ConstraintType.PARALLEL |
static Sketch.ConstraintType |
Sketch.ConstraintType.PARALLEL_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.PATTERN |
static Sketch.ConstraintType |
Sketch.ConstraintType.PERIMETER_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.PERPENDICULAR |
static Sketch.ConstraintType |
Sketch.ConstraintType.PERPENDICULAR_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.POINT_ON_CURVE |
static Sketch.ConstraintType |
Sketch.ConstraintType.POINT_ON_LOOP |
static Sketch.ConstraintType |
Sketch.ConstraintType.POINT_ON_STRING |
static Sketch.ConstraintType |
Sketch.ConstraintType.RADIUS_DIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.RECIPE_TRIM |
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON1
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON2
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON3
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON4
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON5
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.RESERVED_CON6
Do not use
|
static Sketch.ConstraintType |
Sketch.ConstraintType.SLOPE |
static Sketch.ConstraintType |
Sketch.ConstraintType.TANGENT |
static Sketch.ConstraintType |
Sketch.ConstraintType.UNIFORM_SCALED |
static Sketch.ConstraintType |
Sketch.ConstraintType.VERTICAL |
static Sketch.ConstraintType |
Sketch.ConstraintType.VERTICAL_DIM |
Modifier and Type | Method and Description |
---|---|
Sketch.ConstraintType |
SketchConstraint.constraintType()
Returns the constraint's type
License requirements: None. |
static Sketch.ConstraintType |
Sketch.ConstraintType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Sketch.ConstraintType |
Sketch.ConstraintType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Sketch.ConstraintType[] |
Sketch.ConstraintType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
SketchConstraint[] |
Sketch.autoConstrain(double linearTolerance,
double angularTolerance,
boolean allowRemoteConstraints,
SmartObject[] geometries,
Sketch.ConstraintType[] autoconstraintTypes)
Creates Automatic Constraints on input set of geometries.
|
SketchDimensionalConstraint |
Sketch.createDimension(Sketch.ConstraintType dimType,
Sketch.DimensionGeometry dimObject1,
Sketch.DimensionGeometry dimObject2,
Point3d dimOrigin,
Expression expression)
Creates a dimension between two geometric objects.
|
SketchDimensionalConstraint |
Sketch.createDimension(Sketch.ConstraintType dimType,
Sketch.DimensionGeometry dimObject1,
Sketch.DimensionGeometry dimObject2,
Point3d dimOrigin,
Expression expression,
Sketch.DimensionOption refDim)
Creates a dimension between two geometric objects.
|
SketchConstraint[] |
Sketch.getAllConstraintsOfType(Sketch.ConstraintClass conClass,
Sketch.ConstraintType conType)
Gets all constraints in the sketch of a particular type
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.