Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Interface and Description |
---|---|
interface |
CavityMilling
Represents a Cavity Milling Operation
To create or edit an instance of this class, use CavityMillingBuilder Created in NX7.5.0 |
interface |
CenterlineDrillTurning
Represents a Centerline Drill Turning operation
To create or edit an instance of this class, use CenterlineDrillTurningBuilder Created in NX7.5.0 |
interface |
ChamferMilling
Represents a Chamfer Milling Operation
To create or edit an instance of this class, use ChamferMillingBuilder Created in NX9.0.2 |
interface |
CylinderMilling
Represents a Cylinder Milling Operation
To create or edit an instance of this class, use CylinderMillingBuilder Created in NX9.0.1 |
interface |
Documentation
Represents a Documentation operation
To create or edit an instance of this class, use DocumentationBuilder Created in NX9.0.3 |
interface |
Engraving
Represents a Engraving Operation
To create or edit an instance of this class, use EngravingBuilder Created in NX7.5.0 |
interface |
FaceMilling
Represents a Face Milling Operation
To create or edit an instance of this class, use FaceMillingBuilder Created in NX7.5.0 |
interface |
FeatureMilling
Represents a Feature Milling Operation
To create or edit an instance of this class, use FeatureMillingBuilder Created in NX7.5.0 |
interface |
FinishTurning
Represents a Turn Finishing operation
To create or edit an instance of this class, use FinishTurningBuilder Created in NX7.5.0 |
interface |
GenericMotionControl
Represents a Generic Motion Control operation
To create or edit an instance of this class, use GmcOpBuilder Created in NX7.5.0 |
interface |
GrooveMilling
Represents a Groove Milling Operation
To create or edit an instance of this class, use GrooveMillingBuilder Created in NX9.0.0 |
interface |
HoleDrilling
Represents a Hole Drilling Operation
To create or edit an instance of this class, use HoleDrillingBuilder Created in NX9.0.1 |
interface |
HoleMaking
Represents a Hole Making operation
To create or edit an instance of this class, use HoleMakingBuilder Created in NX7.5.0 |
interface |
InspectionOperation
Represents an Inspection operation
To obtain an instance of this class use InspectionOperationCollection Created in NX7.0.0 |
interface |
LatheMachineControl
Represents a Lathe Machine Control operation
To create or edit an instance of this class, use LatheMachineControlBuilder Created in NX7.5.0 |
interface |
LatheUserDefined
Represents a Lathe User Defined operation
To create or edit an instance of this class, use LatheUserDefinedBuilder Created in NX7.5.0 |
interface |
ManualControl
Represents a ManualControl operation
To create or edit an instance of this class, use ManualControlBuilder Created in NX10.0.3 |
interface |
MillMachineControl
Represents a Mill Machine Control operation
To create or edit an instance of this class, use MillMachineControlBuilder Created in NX7.5.0 |
interface |
MillOperation
Represents a Mill operation
To create or edit an instance of this class, use MillOperationBuilder Created in NX7.5.0 |
interface |
MillToolProbing
Represents a Mill Tool operation
To create or edit an instance of this class, use MillToolProbingBuilder Created in NX8.5.1 |
interface |
MillUserDefined
Represents a Mill User Defined operation
To create or edit an instance of this class, use MillUserDefinedBuilder Created in NX7.5.0 |
interface |
PlanarMilling
Represents a Planar Milling Operation
To create or edit an instance of this class, use PlanarMillingBuilder Created in NX7.5.0 |
interface |
PlanarOperation
Represents a Planar operation
To create or edit an instance of this class, use PlanarOperationBuilder Created in NX7.5.0 |
interface |
PlungeMilling
Represents a Plunge Milling Operation
To create or edit an instance of this class, use PlungeMillingBuilder Created in NX7.5.0 |
interface |
RadialGrooveMilling
Represents a Radial Groove Milling Operation
To create or edit an instance of this class, use RadialGrooveMillingBuilder Created in NX9.0.3 |
interface |
RoughFinishTurning
Represents a Turn Rough Finish operation
To create or edit an instance of this class, use RoughFinishTurningBuilder Created in NX7.5.0 |
interface |
RoughTurning
Represents a Turn Rough operation
To create or edit an instance of this class, use RoughTurningBuilder Created in NX7.5.0 |
interface |
SurfaceContour
Represents a Surface Contour operation
To create or edit an instance of this class, use SurfaceContourBuilder Created in NX7.5.0 |
interface |
TeachmodeTurning
Represents a Turning Teachmode operation
To create or edit an instance of this class, use TeachmodeTurningBuilder Created in NX7.5.0 |
interface |
ThreadMilling
Represents a Thread Milling Operation
To create or edit an instance of this class, use ThreadMillingBuilder Created in NX7.5.0 |
interface |
ThreadTurning
Represents a Thread Turning operation
To create or edit an instance of this class, use ThreadTurningBuilder Created in NX7.5.0 |
interface |
TurningOperation
Represents a Turning operation
To create or edit an instance of this class, use TurningOperationBuilder Created in NX7.5.0 |
interface |
TurnPartProbing
Represents a Turn Part Probing operation
To create or edit an instance of this class, use TurnPartProbingBuilder Created in NX8.5.1 |
interface |
TurnToolProbing
Represents a Turn tool operation
To create or edit an instance of this class, use TurnToolProbingBuilder Created in NX8.5.1 |
interface |
UserDefinedOpr
Represents a User Defined operation
To create or edit an instance of this class, use UserDefinedOprBuilder Created in NX7.5.0 |
interface |
VariableZLevelMilling
Represents a Variable Z Level Milling Operation
To create or edit an instance of this class, use VazlMillingBuilder Created in NX7.5.0 |
interface |
VolumeBased25DMillingOperation
Represents a Floor Wall Milling Operation
To create or edit an instance of this class, use VolumeBased25DMillingOperationBuilder Created in NX8.5.0 |
interface |
WedmMachineControl
Represents a WEDM Machine Control operation
To create or edit an instance of this class, use WedmMachineControlBuilder Created in NX7.5.0 |
interface |
WedmUserDefined
Represents a User Defined WEDM operation
To create or edit an instance of this class, use WedmUserDefinedBuilder Created in NX7.5.0 |
interface |
ZLevelMilling
Represents a Z Level Milling Operation
To create or edit an instance of this class, use ZLevelMillingBuilder Created in NX7.5.0 |
Modifier and Type | Field and Description |
---|---|
Operation[] |
FeatureProcessBuilder.CreateFeatureProcessesData.operations
List with created operations,
|
Operation[] |
FeatureProcessBuilder.RecreateFeatureProcessesData.operations
List with created operations,
|
Modifier and Type | Method and Description |
---|---|
Operation |
OperationCollection.create(NCGroup parentProgramGroup,
NCGroup parentMethodGroup,
NCGroup parentToolGroup,
NCGroup parentGeometryGroup,
String typeName,
String subtypeName,
OperationCollection.UseDefaultName useDefaultName,
String newOperationName)
Create an operation of the specified type and subtype under the parent groups.
|
Operation |
OperationCollection.findObject(String sid)
Finds the CAM.Operation object with the given identifier as recorded in a journal.
|
Operation[] |
Operation.getDividedOperations()
Get the divided operations from tool path divide of this operation
License requirements: cam_base ("CAM BASE") . |
Operation |
Operation.getFirstOfDivide()
Get the first source operation of the divided operation
License requirements: cam_base ("CAM BASE") . |
Operation[] |
OperationTeaching.getOperations()
Gets the selected operations
License requirements: fbm_author ("FBM Author") . |
Operation[] |
FeatureGeometryGroup.getOperations()
Get the operations of the feature group
License requirements: None. |
Operation[] |
CAMFeature.getOperations()
Get the operations manufacturing the CAMFeature
License requirements: None. |
Operation[] |
Operation.getOtherInstances()
Get the other instances of the operation
License requirements: cam_base ("CAM BASE") . |
Operation |
ToolPathSplitItemBuilder.operation()
Returns the operation object returned
License requirements: None. |
Operation |
CutDepthChecker.operationToCheck()
Returns the operation that is being checked
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
OperationTeaching.setOperations(Operation[] aOperations)
Sets the selected operations
License requirements: fbm_author ("FBM Author") . |
void |
CutDepthChecker.setOperationToCheck(Operation operation)
License requirements: cam_base ("CAM BASE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.