Package | Description |
---|---|
nxopen.cam |
Provides classes and interfaces for Manufacturing.
|
Modifier and Type | Field and Description |
---|---|
static InspectionConstructedFeatureBuilder.DesignCreationType |
InspectionConstructedFeatureBuilder.DesignCreationType.CREATE_NEW
Design feature is created as a new feature
|
static InspectionConstructedFeatureBuilder.DesignCreationType |
InspectionConstructedFeatureBuilder.DesignCreationType.SELECT_EXISTING
Design feature is selected from existing features
|
Modifier and Type | Method and Description |
---|---|
InspectionConstructedFeatureBuilder.DesignCreationType |
InspectionConstructedFeatureBuilder.designCreation()
Returns the design feature creation type
License requirements: None. |
static InspectionConstructedFeatureBuilder.DesignCreationType |
InspectionConstructedFeatureBuilder.DesignCreationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.DesignCreationType |
InspectionConstructedFeatureBuilder.DesignCreationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.DesignCreationType[] |
InspectionConstructedFeatureBuilder.DesignCreationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
InspectionConstructedFeatureBuilder.setDesignCreation(InspectionConstructedFeatureBuilder.DesignCreationType creationType)
License requirements: insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.