public static class InspectionConstructedFeatureBuilder.DesignCreationType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CREATE_NEW
Design feature is created as a new feature
|
static int |
_SELECT_EXISTING
Design feature is selected from existing features
|
static InspectionConstructedFeatureBuilder.DesignCreationType |
CREATE_NEW
Design feature is created as a new feature
|
static InspectionConstructedFeatureBuilder.DesignCreationType |
SELECT_EXISTING
Design feature is selected from existing features
|
Modifier and Type | Method and Description |
---|---|
static InspectionConstructedFeatureBuilder.DesignCreationType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static InspectionConstructedFeatureBuilder.DesignCreationType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static InspectionConstructedFeatureBuilder.DesignCreationType[] |
values()
Returns an array that contains the values for this enum.
|
public static final InspectionConstructedFeatureBuilder.DesignCreationType SELECT_EXISTING
public static final InspectionConstructedFeatureBuilder.DesignCreationType CREATE_NEW
public static final int _SELECT_EXISTING
public static final int _CREATE_NEW
public static InspectionConstructedFeatureBuilder.DesignCreationType valueOf(int value)
public static InspectionConstructedFeatureBuilder.DesignCreationType valueOf(String name)
public static InspectionConstructedFeatureBuilder.DesignCreationType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.