Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.cae.aerostructures |
Provides classes and interfaces relating to Aero Structures.
|
nxopen.cae.optimization |
Provides classes and interfaces relating to Optimization.
|
nxopen.cae.responsesimulation |
Provides classes and interfaces for Response Simulation.
|
Modifier and Type | Field and Description |
---|---|
SimSolution[] |
SimSolveManager.ChainOfPrerequisitesData.psolutions
the prerequisites of the input solution
|
Modifier and Type | Method and Description |
---|---|
SimSolution |
SimSimulation.activeSolution()
Returns the active solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
SimSimulation.cloneSolution(SimSolution oldSolution,
String suggestedName)
Clone the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
SimSimulation.createSolution(NodalForceReport nodalForceReport,
String name,
NodalForceReport.SubcaseOption subcaseOption,
SimSolutionStep stepTag,
boolean createForce,
boolean createMoment)
Creates a solution from free body
License requirements: nx_masterfem ("Finite Element Modeling") . |
SimSolution |
SimSimulation.createSolution(SimConditionSequence conditionSeqeunce,
double stepSize,
Unit stepUnit,
String solverType,
String analysisType,
String solutionType,
String name)
Deprecated.
Deprecated in NX11.0.0. Use
SimSimulation.createSolution(java.lang.String, java.lang.String, java.lang.String, java.lang.String) and setTimePropsFromConditionSequence(nxopen.cae.SimConditionSequence) with step size input instead.
|
SimSolution |
SimSimulation.createSolution(SimConditionSequence conditionSeqeunce,
int numSteps,
String solverType,
String analysisType,
String solutionType,
String name)
Deprecated.
Deprecated in NX11.0.0. Use
SimSimulation.createSolution(java.lang.String, java.lang.String, java.lang.String, java.lang.String) and setTimePropsFromConditionSequence(nxopen.cae.SimConditionSequence) with number of steps input instead.
|
SimSolution |
SimSimulation.createSolution(SimConditionSequence conditionSeqeunce,
String solverType,
String analysisType,
String solutionType,
String name)
Deprecated.
Deprecated in NX11.0.0. Use
SimSimulation.createSolution(java.lang.String, java.lang.String, java.lang.String, java.lang.String) and setTimePropsFromConditionSequence(nxopen.cae.SimConditionSequence) instead.
|
SimSolution |
SimSimulation.createSolution(String solverType,
String analysisType,
String solutionType,
String name)
Deprecated.
Deprecated in NX11.0.0. Use
SimSimulation.createSolution(java.lang.String, java.lang.String, java.lang.String, java.lang.String) with abstraction type input instead.
|
SimSolution |
SimSimulation.createSolution(String solverType,
String analysisType,
String solutionType,
String name,
SimSimulation.AxisymAbstractionType abstractionType)
Creates a solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
MechanicalLoadSumBuilder.getSolution()
The solution object
License requirements: None. |
SimSolution |
CorrelSolutionBuilder.referenceSolution()
Returns the reference (test) solution of correlation
License requirements: None. |
SimSolution |
SolutionResult.solution()
Returns the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
SmoothOptResultsBuilder.solution()
Returns the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
SimSolutionStep.solution()
Returns the solution to which the step belongs
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
PreTestSolutionBuilder.solution()
Returns the pre-test working solution
License requirements: None. |
SimSolution |
LaminateDynamicSimBuilder.solution()
Returns the solution
License requirements: None. |
SimSolution |
CorrelSolutionBuilder.workSolution()
Returns the work (analysis) solution of correlation
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
SimSimulation.addBc(SimBC bc,
SimSolution solution,
SimSolutionStep solutionStep)
Adds the boundary condition to the step in the solution passed.
|
void |
SolutionManager.addBc(SimSolution tSolution,
SimBC tBc)
Add bc to a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.addFolder(SimSolution tSolution,
SimLbcFolder tBc)
Add bc folder to a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.addLoadset(SimSolution tSolution,
SimLoadSet tBc)
Add loadset to a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SimSolution.addPrerequisite(SimSolution prerequisite)
Adds a prerequisite to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
SimSolution |
SimSimulation.cloneSolution(SimSolution oldSolution,
String suggestedName)
Clone the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
SolutionResult.combineLoadcases(SimPart part,
SimSolution solution,
SimSolutionStep[] lcaseas,
double[] factors,
String desc)
Deprecated.
Deprecated in NX10.0.0. Use overloaded function with Result Reference instead.
|
ResultProbe |
ResultProbe.copyToSolution(SimSolution targetSolution)
Copy the result probe to target solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
CorrelApplyAlignmentFromBuilder |
CorrelManager.createCorrelApplyAlignmentFromBuilder(SimSolution solution)
Creates a
CorrelApplyAlignmentFromBuilder
License requirements: nx_correl_base ("FE Correlation") Created in NX9.0.0 |
CorrelFineTuneAlignmentBuilder |
CorrelManager.createCorrelFineTuneAlignmentBuilder(SimSolution solution)
Creates a
CorrelFineTuneAlignmentBuilder
License requirements: nx_correl_base ("FE Correlation") Created in NX9.0.0 |
ResultMeasureResultOptions |
ResultMeasureCollection.createNewResultOptions(SimSolution tSol,
SimResultReference tResultReference,
Loadcase tResultLoadcase,
Iteration tResultIteration,
boolean bAllSubiterations,
Iteration tResultSubIteration,
Result.Type pType,
Result.Component eComp)
Create a result options for result measure
License requirements: nx_masterfem ("Finite Element Modeling") . |
ResultMeasure |
ResultMeasureCollection.createResultMeasure(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp,
String expName)
Deprecated.
Deprecated in NX10.0.0. Use
ResultMeasureCollection.createResultMeasureNew(nxopen.cae.ResultMeasureResultOptions, nxopen.cae.ResultMeasureModelSubset, java.lang.String) instead.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptions(SimSolution tSol,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
Deprecated.
|
ResultMeasureResultOptions |
ResultMeasureCollection.createResultOptionsNew(SimSolution tSol,
SimResultReference tResultReference,
int iStepIndex,
int iIterIndex,
Result.Type pType,
Result.Component eComp)
|
SolutionResult |
ResultManager.createSolutionResult(SimSolution solution)
Creates a solution result object given a
SimSolution
It is user's responsibility to destroy the result object once done
using ResultManager.deleteResult(nxopen.cae.Result) , in order to free up system resources. |
SimSolutionStep |
SimSimulation.createSolutionStep(SimSolution solution,
int stepType,
String name)
Creates a step and add to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
StepManager |
SimSimulation.createStepManager(SimSolution tSol)
Creates a
StepManager for a solution
License requirements: nx_masterfem ("Finite Element Modeling") Created in NX10.0.0 |
void |
SimSimulation.deleteSolution(SimSolution solution)
Delete the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
SimLoadRecipeLbcGenerator.generate(SimSolution solution)
Deprecated.
Deprecated in NX11.0.0. Use method taking LBC hierarchy type as input. This method always creates separated LBCs.
|
void |
SimLoadRecipeLbcGenerator.generate(SimSolution solution,
int stepType)
Deprecated.
Deprecated in NX11.0.0. Use method taking LBC hierarchy type as input. This method always creates separated LBCs.
|
void |
SimLoadRecipeLbcGenerator.generate(SimSolution solution,
int stepType,
SimLoadRecipeLbcGenerator.LbcHierarchyTypes lbcHierarchyType)
Generates Loads at the level of solution steps.
|
void |
SimLoadRecipeLbcGenerator.generate(SimSolution solution,
SimLoadRecipeLbcGenerator.LbcHierarchyTypes lbcHierarchyType)
Generates Loads at solution level.
|
int |
SimLoadRecipeLbcGenerator.getAllowedStepTypeCount(SimSolution solution)
Gets the count of allowable step types when generating steps for a solution from a load recipe.
|
SimSolveManager.ChainOfPrerequisitesData |
SimSolveManager.getChainOfPrerequisites(SimSolution pSol)
Return the chain of prerequisites for the given solution.
|
int |
Post.loadSolutionResult(SimSolution solution)
Deprecated.
Deprecated in NX11.0.0. Use
ResultManager.createSolutionResult(nxopen.cae.SimSolution) instead.
|
void |
SolutionManager.removeBc(SimSolution tSolution,
SimBC tBc)
Remove bc from a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.removeFolder(SimSolution tSolution,
SimLbcFolder tBc)
Remove bc folder from a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.removeLoadset(SimSolution tSolution,
SimLoadSet tBc)
Remove loadset from a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SimSolution.removePrerequisite(SimSolution prerequisite)
Remove a prerequisite to the solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
SolutionManager.scaleBc(SimSolution tSolution,
SimBC tBc,
double scale)
Set scale factor on bc in a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.scaleFolder(SimSolution tSolution,
SimLbcFolder tBc,
double scale)
Set scale factor on bc folder in a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SolutionManager.scaleLoadset(SimSolution tSolution,
SimLoadSet tBc,
double scale)
Set scale factor on loadset in a solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
SimSimulation.setActiveSolution(SimSolution activeSolution)
Sets the active solution
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
ResultsManipulationBuilder.setCompanionSolution(SimSolution solution)
Deprecated.
Deprecated in NX10.0.0. Use
ResultsManipulationBuilder.setCompanionResultReference(nxopen.cae.SimResultReference) instead.
|
void |
CorrelSolutionBuilder.setReferenceSolution(SimSolution referenceSolution)
License requirements: nx_correl_base ("FE Correlation") . |
void |
SmoothOptResultsBuilder.setSolution(SimSolution solution)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
PreTestSolutionBuilder.setSolution(SimSolution solution)
License requirements: nx_correl_base ("FE Correlation") . |
void |
MechanicalLoadSumBuilder.setSolution(SimSolution solution)
The solution object
License requirements: nx_masterfem ("Finite Element Modeling") . |
void |
LaminateDynamicSimBuilder.setSolution(SimSolution solution)
License requirements: nx_lam_comp_adv ("Laminate Composites Advanced") . |
void |
ImportSimulationBuilder.setSolutions(SimSolution[] solutions)
Set solutions to import
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
CorrelSolutionBuilder.setWorkSolution(SimSolution workSolution)
License requirements: nx_correl_base ("FE Correlation") . |
SimSolveManager.SolveChainOfSolutionsData |
SimSolveManager.solveChainOfSolutions(SimSolution[] pSolutions,
SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption)
Solve the chain of solutions given in input.
|
void |
PreTestSolution.updateResultsForSolution(SimSolution tSolution,
boolean ignoreReload)
Update results for pre-test solution
License requirements: nx_correl_base ("FE Correlation") . |
void |
CorrelSolution.updateResultsForSolution(SimSolution tSolution,
boolean ignoreReload)
Update results for correlation solution
License requirements: nx_correl_base ("FE Correlation") . |
Modifier and Type | Method and Description |
---|---|
SimSolution |
MarginSolutionBuilder.referenceSolution()
Returns the referenced FE-Solution of the AeroStructure solution
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
void |
MarginSolutionBuilder.setReferenceSolution(SimSolution referenceSolution)
License requirements: nx_masterfem ("Finite Element Modeling") . |
Modifier and Type | Method and Description |
---|---|
SimSolution |
DAOSolutionBuilder.analysisSolution()
Returns the optimization solution analysis solution
License requirements: None. |
SimSolution |
TBSOptimizationSolutionBuilder.referencedSolution()
Returns the referenced solution
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
DAOSolutionBuilder.setAnalysisSolution(SimSolution analysisSolution)
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") . |
void |
TBSOptimizationSolutionBuilder.setReferencedSolution(SimSolution referencedSolution)
License requirements: cae_opt_topo ("NX Topology Optimization") OR cae_opt_topobead ("NX Bead Optimization") OR cae_opt_toposhape ("NX Shape Optimization") . |
Modifier and Type | Method and Description |
---|---|
SimSolution |
SolutionBuilder.referencedSolution()
Returns the referenced solution which must be a SEMODES *103 solution with modal results solved
License requirements: nx_response_anlys ("NX Response Analysis") . |
Modifier and Type | Method and Description |
---|---|
void |
SolutionBuilder.setReferencedSolution(SimSolution referencedSolution)
License requirements: nx_response_anlys ("NX Response Analysis") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.