public static class SimSolution.SetupCheckOption extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CHECK_AND_STOP_AT_FIRST_ERROR
perform set up checks but stop at first error
|
static int |
_COMPLETE_CHECK_AND_OUTPUT_ERRORS
perform all set up checks and report all errors
|
static int |
_DO_NOT_CHECK
do perform any set up checks
|
static SimSolution.SetupCheckOption |
CHECK_AND_STOP_AT_FIRST_ERROR
perform set up checks but stop at first error
|
static SimSolution.SetupCheckOption |
COMPLETE_CHECK_AND_OUTPUT_ERRORS
perform all set up checks and report all errors
|
static SimSolution.SetupCheckOption |
DO_NOT_CHECK
do perform any set up checks
|
Modifier and Type | Method and Description |
---|---|
static SimSolution.SetupCheckOption |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SimSolution.SetupCheckOption |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SimSolution.SetupCheckOption[] |
values()
Returns an array that contains the values for this enum.
|
public static final SimSolution.SetupCheckOption DO_NOT_CHECK
public static final SimSolution.SetupCheckOption CHECK_AND_STOP_AT_FIRST_ERROR
public static final SimSolution.SetupCheckOption COMPLETE_CHECK_AND_OUTPUT_ERRORS
public static final int _DO_NOT_CHECK
public static final int _CHECK_AND_STOP_AT_FIRST_ERROR
public static final int _COMPLETE_CHECK_AND_OUTPUT_ERRORS
public static SimSolution.SetupCheckOption valueOf(int value)
public static SimSolution.SetupCheckOption valueOf(String name)
public static SimSolution.SetupCheckOption[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.