public interface SimSolveManager extends Remote
SimSolveManager
manager which is used to manage the solve process of solutions.
Session
Modifier and Type | Interface and Description |
---|---|
static class |
SimSolveManager.ChainOfPrerequisitesData
This class holds the data returned from
getChainOfPrerequisites(nxopen.cae.SimSolution) |
static class |
SimSolveManager.SolveAllMetaSolutionsData
This class holds the data returned from
solveAllMetaSolutions(nxopen.cae.SimSolution.SolveOption, nxopen.cae.SimSolution.SetupCheckOption, nxopen.cae.SimSolution.SolveMode, boolean) |
static class |
SimSolveManager.SolveAllSolutionsData
This class holds the data returned from
solveAllSolutions(nxopen.cae.SimSolution.SolveOption, nxopen.cae.SimSolution.SetupCheckOption, nxopen.cae.SimSolution.SolveMode, boolean) |
static class |
SimSolveManager.SolveChainOfSolutionsData
This class holds the data returned from
solveChainOfSolutions(nxopen.cae.SimSolution[], nxopen.cae.SimSolution.SolveOption, nxopen.cae.SimSolution.SetupCheckOption, nxopen.cae.SimSolution.SolveMode) |
Modifier and Type | Method and Description |
---|---|
SimSolveManager.ChainOfPrerequisitesData |
getChainOfPrerequisites(SimSolution pSol)
Return the chain of prerequisites for the given solution.
|
SimSolveManager.SolveAllMetaSolutionsData |
solveAllMetaSolutions(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption,
boolean skipSolutionWithResults)
Solve all meta solutions in the sim document.
|
SimSolveManager.SolveAllSolutionsData |
solveAllSolutions(SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption,
boolean skipSolutionWithResults)
Solve all solutions in the sim document.
|
SimSolveManager.SolveChainOfSolutionsData |
solveChainOfSolutions(SimSolution[] pSolutions,
SimSolution.SolveOption solveOption,
SimSolution.SetupCheckOption setupCheckOption,
SimSolution.SolveMode runModeOption)
Solve the chain of solutions given in input.
|
SimSolveManager.ChainOfPrerequisitesData getChainOfPrerequisites(SimSolution pSol) throws NXException, RemoteException
pSol
- the solution for which we want the chain of prerequisitesNXException
RemoteException
SimSolveManager.SolveChainOfSolutionsData solveChainOfSolutions(SimSolution[] pSolutions, SimSolution.SolveOption solveOption, SimSolution.SetupCheckOption setupCheckOption, SimSolution.SolveMode runModeOption) throws NXException, RemoteException
pSolutions
- The solutions to be solvedsolveOption
- solve optionsetupCheckOption
- setup check optionrunModeOption
- run mode optionNXException
RemoteException
SimSolveManager.SolveAllSolutionsData solveAllSolutions(SimSolution.SolveOption solveOption, SimSolution.SetupCheckOption setupCheckOption, SimSolution.SolveMode runModeOption, boolean skipSolutionWithResults) throws NXException, RemoteException
solveOption
- solve optionsetupCheckOption
- setup check optionrunModeOption
- run mode optionskipSolutionWithResults
- skip the solution if it has a resultNXException
RemoteException
SimSolveManager.SolveAllMetaSolutionsData solveAllMetaSolutions(SimSolution.SolveOption solveOption, SimSolution.SetupCheckOption setupCheckOption, SimSolution.SolveMode runModeOption, boolean skipSolutionWithResults) throws NXException, RemoteException
solveOption
- solve optionsetupCheckOption
- setup check optionrunModeOption
- run mode optionskipSolutionWithResults
- skip the solution if it has a resultNXException
RemoteException
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.