SketchCollection Class¶
-
class
NXOpen.
SketchCollection
¶ Bases:
object
Represents a collection of sketches
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX3.0.0.
Methods¶
Method Detail¶
CreateAngularDimensionBuilder¶
-
SketchCollection.
CreateAngularDimensionBuilder
¶ Creates a
NXOpen.SketchAngularDimensionBuilder
Signature
CreateAngularDimensionBuilder(angularDimension)
Parameters: angularDimension – the angular dimension to be edited, if None. then create an angular dimension :type angularDimension:
NXOpen.Annotations.AngularDimension
:returns: the angular dimension builder :rtype:NXOpen.SketchAngularDimensionBuilder
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateAutoConstrainBuilder¶
-
SketchCollection.
CreateAutoConstrainBuilder
¶ Creates a
NXOpen.SketchAutoConstrainBuilder
Signature
CreateAutoConstrainBuilder()
Returns: Sketch Auto-Constrain Builder object Return type: NXOpen.SketchAutoConstrainBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateAutoDimensionBuilder¶
-
SketchCollection.
CreateAutoDimensionBuilder
¶ Creates a
NXOpen.SketchAutoDimensionBuilder
Signature
CreateAutoDimensionBuilder()
Returns: Sketch Auto-Dimension Builder object Return type: NXOpen.SketchAutoDimensionBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateConstraintBuilder¶
-
SketchCollection.
CreateConstraintBuilder
¶ Creates a
NXOpen.SketchConstraintBuilder
Signature
CreateConstraintBuilder()
Returns: Return type: NXOpen.SketchConstraintBuilder
New in version NX8.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateConvertToFromReferenceBuilder¶
-
SketchCollection.
CreateConvertToFromReferenceBuilder
¶ Creates a
NXOpen.ConvertToFromReferenceBuilder
Signature
CreateConvertToFromReferenceBuilder()
Returns: Sketch ConvertToFromReferenceBuilder object Return type: NXOpen.ConvertToFromReferenceBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateCornerBuilder¶
-
SketchCollection.
CreateCornerBuilder
¶ Creates a
NXOpen.SketchCornerBuilder
Signature
CreateCornerBuilder()
Returns: CornerBuilder object Return type: NXOpen.SketchCornerBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateDimensionBuilder¶
-
SketchCollection.
CreateDimensionBuilder
¶ Creates a
NXOpen.SketchDimensionBuilder
Signature
CreateDimensionBuilder(constraint)
Parameters: constraint ( NXOpen.SketchDimensionalConstraint
) – The sketch dimensional constraint to be edited.Returns: DimensionBuilder object Return type: NXOpen.SketchDimensionBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateEditDefiningSectionBuilder¶
-
SketchCollection.
CreateEditDefiningSectionBuilder
¶ Creates a
NXOpen.SketchEditDefiningSectionBuilder
Signature
CreateEditDefiningSectionBuilder()
Returns: Edit Defining Section Builder object Return type: NXOpen.SketchEditDefiningSectionBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateInferredConstraintsBuilder¶
-
SketchCollection.
CreateInferredConstraintsBuilder
¶ Creates a
NXOpen.InferredConstraintsBuilder
Signature
CreateInferredConstraintsBuilder()
Returns: InferredConstraintsBuilder object Return type: NXOpen.InferredConstraintsBuilder
New in version NX5.0.0.
License requirements: None.
CreateIntersectionCurveBuilder¶
-
SketchCollection.
CreateIntersectionCurveBuilder
¶ Creates the builder for intersection curve
Signature
CreateIntersectionCurveBuilder(operation)
Parameters: operation ( NXOpen.SketchIntersectionCurve
) –Returns: Return type: NXOpen.SketchIntersectionCurveBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateIntersectionPointBuilder¶
-
SketchCollection.
CreateIntersectionPointBuilder
¶ Creates the builder for intersection point
Signature
CreateIntersectionPointBuilder(operation)
Parameters: operation ( NXOpen.SketchIntersectionPoint
) –Returns: Return type: NXOpen.SketchIntersectionPointBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateLinearDimensionBuilder¶
-
SketchCollection.
CreateLinearDimensionBuilder
¶ Creates a
NXOpen.SketchLinearDimensionBuilder
Signature
CreateLinearDimensionBuilder(linearDimension)
Parameters: linearDimension ( NXOpen.Annotations.Dimension
) – the linear dimension to be edited, if None, then create a linear dimensionReturns: the linear dimension builder Return type: NXOpen.SketchLinearDimensionBuilder
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateMakeSymmetricBuilder¶
-
SketchCollection.
CreateMakeSymmetricBuilder
¶ Creates a
NXOpen.SketchMakeSymmetricBuilder
Signature
CreateMakeSymmetricBuilder()
Returns: MakeSymmetricBuilder object Return type: NXOpen.SketchMakeSymmetricBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateNewSketchInPlaceBuilder¶
-
SketchCollection.
CreateNewSketchInPlaceBuilder
¶ Creates a
NXOpen.SketchInPlaceBuilder
Signature
CreateNewSketchInPlaceBuilder(operation)
Parameters: operation ( NXOpen.Sketch
) – TheNXOpen.Sketch
to reattach or None to create a new oneReturns: SketchInPlaceBuilder object Return type: NXOpen.SketchInPlaceBuilder
New in version NX7.5.0.
Deprecated since version NX11.0.0: Use
NXOpen.SketchCollection.CreateSketchInPlaceBuilder2()
instead.License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateProjectBuilder¶
-
SketchCollection.
CreateProjectBuilder
¶ Creates a
NXOpen.SketchProjectBuilder
Signature
CreateProjectBuilder(operation)
Parameters: operation ( NXOpen.Features.Feature
) – The feature for theNXOpen.SketchProjectBuilder
to be edited, if None then create a new oneReturns: ProjectBuilder object Return type: NXOpen.SketchProjectBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateQuickExtendBuilder¶
-
SketchCollection.
CreateQuickExtendBuilder
¶ Creates a
NXOpen.SketchQuickExtendBuilder
Signature
CreateQuickExtendBuilder()
Returns: Sketch Quick-Extend Builder object Return type: NXOpen.SketchQuickExtendBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateQuickTrimBuilder¶
-
SketchCollection.
CreateQuickTrimBuilder
¶ Creates a
NXOpen.SketchQuickTrimBuilder
Signature
CreateQuickTrimBuilder()
Returns: Sketch QuickTrim Builder object Return type: NXOpen.SketchQuickTrimBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateRadialDimensionBuilder¶
-
SketchCollection.
CreateRadialDimensionBuilder
¶ Creates a
NXOpen.SketchRadialDimensionBuilder
Signature
CreateRadialDimensionBuilder(radialDimension)
Parameters: radialDimension ( NXOpen.Annotations.Dimension
) – the radial dimension to be edited, if None, then create a radial dimensionReturns: the radial dimension builder Return type: NXOpen.SketchRadialDimensionBuilder
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateRapidDimensionBuilder¶
-
SketchCollection.
CreateRapidDimensionBuilder
¶ Creates a
NXOpen.SketchRapidDimensionBuilder
Signature
CreateRapidDimensionBuilder()
Returns: the rapid dimension builder Return type: NXOpen.SketchRapidDimensionBuilder
New in version NX9.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
CreateSketch¶
-
SketchCollection.
CreateSketch
¶ Overloaded method CreateSketch
CreateSketch(name, attachmentPlane, referenceAxis, referenceDirection, referenceAxisOrientation, referenceAxisSense, normalOrientation)
CreateSketch(name, attachmentPlane, referenceAxis, referenceDirection, referenceAxisOrientation, referenceAxisSense, normalOrientation, view)
-------------------------------------
Creates a sketch
Signature
CreateSketch(name, attachmentPlane, referenceAxis, referenceDirection, referenceAxisOrientation, referenceAxisSense, normalOrientation)
Parameters: - name (str) – Name of the sketch. The name will be converted to upper case. If this is an empty string or None, a name will be provided by the system.
- attachmentPlane (
NXOpen.ISurface
) – A face or datum plane that the sketch will be attached to. Must be planar. - referenceAxis (
NXOpen.IReferenceAxis
) – Can be a datum axis, edge, datum plane, face, or NXOpen.IReferenceAxis.NULL. If it is an edge, the edge must be a line segment. If it is a face, the face must be a plane. If NXOpen.IReferenceAxis.NULL, the reference_direction is used instead - referenceDirection (
NXOpen.Vector3d
) – If reference_axis is None, this parameter sets the reference direction of the sketch. In this case, this parameter must not be (0,0,0). If reference_axis is not None and this parameter is not (0,0,0), this parameter determines whether the reference direction should be in the same direction as reference_axis or in the opposite direction. If this parameter is (0,0,0), this parameter is not used. - referenceAxisOrientation (
NXOpen.AxisOrientation
) – indicates whether the reference axis is horizontal or vertical - referenceAxisSense (
NXOpen.Sense
) – Ignored unless reference_direction is (0,0,0) and reference_axis is an edge or datum axis. This parameter indicates whether the reference axis should be in the same direction as reference_axis or in the opposite direction - normalOrientation (
NXOpen.PlaneNormalOrientation
) – whether the sketch’s Z-axis should be outward or inward
Returns: the new sketch
Return type: New in version NX3.0.0.
Deprecated since version NX7.5.3: Use
NXOpen.SketchInPlaceBuilder
instead.License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
-------------------------------------
Creates a sketch. This function takes in an argument for the view to create the sketch in a drafting member view.
Signature
CreateSketch(name, attachmentPlane, referenceAxis, referenceDirection, referenceAxisOrientation, referenceAxisSense, normalOrientation, view)
Parameters: - name (str) – Name of the sketch. The name will be converted to upper case. If this is an empty string or None, a name will be provided by the system.
- attachmentPlane (
NXOpen.ISurface
) – A face or datum plane that the sketch will be attached to. Must be planar. - referenceAxis (
NXOpen.IReferenceAxis
) – Can be a datum axis, edge, datum plane, face, or NXOpen.IReferenceAxis.NULL. If it is an edge, the edge must be a line segment. If it is a face, the face must be a plane. If NXOpen.IReferenceAxis.NULL, the reference_direction is used instead - referenceDirection (
NXOpen.Vector3d
) – If reference_axis is None, this parameter sets the reference direction of the sketch. In this case, this parameter must not be (0,0,0). If reference_axis is not None and this parameter is not (0,0,0), this parameter determines whether the reference direction should be in the same direction as reference_axis or in the opposite direction. If this parameter is (0,0,0), this parameter is not used. - referenceAxisOrientation (
NXOpen.AxisOrientation
) – indicates whether the reference axis is horizontal or vertical - referenceAxisSense (
NXOpen.Sense
) – Ignored unless reference_direction is (0,0,0) and reference_axis is an edge or datum axis. This parameter indicates whether the reference axis should be in the same direction as reference_axis or in the opposite direction - normalOrientation (
NXOpen.PlaneNormalOrientation
) – whether the sketch’s Z-axis should be outward or inward - view (
NXOpen.NXObject
) – View of the drafting view in which the sketch needsto be created
Returns: the new sketch
Return type: New in version NX4.0.0.
Deprecated since version NX7.5.3: Use
NXOpen.SketchInDraftingBuilder
instead.License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
-------------------------------------
CreateSketchAlongPathBuilder¶
-
SketchCollection.
CreateSketchAlongPathBuilder
¶ Creates a
NXOpen.SketchAlongPathBuilder
Signature
CreateSketchAlongPathBuilder(operation)
Parameters: operation ( NXOpen.Sketch
) – TheNXOpen.Sketch
to reattach or None to create a new oneReturns: SketchAlongPathBuilder object Return type: NXOpen.SketchAlongPathBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchAssociativeTrimBuilder¶
-
SketchCollection.
CreateSketchAssociativeTrimBuilder
¶ Creates a
NXOpen.SketchAssociativeTrimBuilder
Signature
CreateSketchAssociativeTrimBuilder(trimCon)
Parameters: trimCon ( NXOpen.SketchAssociativeTrim
) – Trim constraintReturns: Return type: NXOpen.SketchAssociativeTrimBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchChamferBuilder¶
-
SketchCollection.
CreateSketchChamferBuilder
¶ Creates a
NXOpen.SketchChamferBuilder
Signature
CreateSketchChamferBuilder()
Returns: Sketch Chamfer Builder object Return type: NXOpen.SketchChamferBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchConicBuilder¶
-
SketchCollection.
CreateSketchConicBuilder
¶ Creates a
NXOpen.SketchConicBuilder
Signature
CreateSketchConicBuilder(conic)
Parameters: conic ( NXOpen.NXObject
) – The conic to be edited.Returns: SketchConicBuilder object Return type: NXOpen.SketchConicBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchEllipseBuilder¶
-
SketchCollection.
CreateSketchEllipseBuilder
¶ Creates a
NXOpen.SketchEllipseBuilder
Signature
CreateSketchEllipseBuilder(ellipse)
Parameters: ellipse ( NXOpen.NXObject
) – The ellipse to be edited.Returns: SketchEllipseBuilder object Return type: NXOpen.SketchEllipseBuilder
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchInDraftingBuilder¶
-
SketchCollection.
CreateSketchInDraftingBuilder
¶ Creates a
NXOpen.SketchInDraftingBuilder
Signature
CreateSketchInDraftingBuilder()
Returns: SketchInDraftingBuilder object Return type: NXOpen.SketchInDraftingBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)
CreateSketchInPlaceBuilder2¶
-
SketchCollection.
CreateSketchInPlaceBuilder2
¶ Creates a
NXOpen.SketchInPlaceBuilder
Signature
CreateSketchInPlaceBuilder2(operation)
Parameters: operation ( NXOpen.Sketch
) – TheNXOpen.Sketch
to reattach or None to create a new oneReturns: SketchInPlaceBuilder object Return type: NXOpen.SketchInPlaceBuilder
New in version NX11.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchMirrorPatternBuilder¶
-
SketchCollection.
CreateSketchMirrorPatternBuilder
¶ Creates a
NXOpen.SketchMirrorPatternBuilder
Signature
CreateSketchMirrorPatternBuilder(con)
Parameters: con ( NXOpen.SketchPattern
) – Pattern constraintReturns: Return type: NXOpen.SketchMirrorPatternBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchOffsetBuilder¶
-
SketchCollection.
CreateSketchOffsetBuilder
¶ Creates a
NXOpen.SketchOffsetBuilder
.This command only supports creation of up to 200 output curves. That means number of curves in input section multiplied by the number of copies must be less than or equal to 200.
Signature
CreateSketchOffsetBuilder(offCon)
Parameters: offCon ( NXOpen.SketchOffset
) – Offset constraintReturns: Return type: NXOpen.SketchOffsetBuilder
New in version NX5.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchPasteBuilder¶
-
SketchCollection.
CreateSketchPasteBuilder
¶ Creates a
NXOpen.SketchPasteBuilder
Signature
CreateSketchPasteBuilder(sketches)
Parameters: sketches (list of NXOpen.Sketch
) –NXOpen.Sketch
to be copy/pasteReturns: Return type: NXOpen.SketchPasteBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchPatternBuilder¶
-
SketchCollection.
CreateSketchPatternBuilder
¶ Creates a
NXOpen.SketchPatternBuilder
Signature
CreateSketchPatternBuilder(con)
Parameters: con ( NXOpen.SketchPattern
) – Pattern constraintReturns: Return type: NXOpen.SketchPatternBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CreateSketchPolygonBuilder¶
-
SketchCollection.
CreateSketchPolygonBuilder
¶ Creates a
NXOpen.SketchPolygonBuilder
Signature
CreateSketchPolygonBuilder(polygonconstraint)
Parameters: polygonconstraint – The polygon constraint. The only acceptable value here is None. :type polygonconstraint:
NXOpen.SketchPolygon
:returns: SketchPolygonBuilder object :rtype:NXOpen.SketchPolygonBuilder
New in version NX7.5.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR geometric_tol (“GDT”)
FindObject¶
-
SketchCollection.
FindObject
¶ Finds the
NXOpen.Sketch
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Sketch
Returns: Sketch with this name Return type: NXOpen.Sketch
New in version NX3.0.0.
License requirements: None.
GetOwningSketch¶
-
SketchCollection.
GetOwningSketch
¶ Returns the sketch that owns the specified geometry
Signature
GetOwningSketch(geometry)
Parameters: geometry ( NXOpen.SmartObject
) –Returns: The sketch that owns the geometry Return type: NXOpen.Sketch
New in version NX4.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”) OR drafting (“DRAFTING”)