SketchConstraintBuilder Class¶
-
class
NXOpen.
SketchConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchConstraint
builderTo create a new instance of this class, use
NXOpen.SketchCollection.CreateConstraintBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
Centerline | Returns the centerline for a symmetric constraint type |
ConstraintType | Returns or sets the constraint type |
GeometryToConstrain | Returns the geometries to be constrained |
GeometryToConstrainTo | Returns the secondary geometries to be constrained |
MakeReference | Returns or sets the flag specifying whether or not to make the centerline reference geometry |
Tag | Returns the Tag for this object. |
UpdateSketchAtCommit | Returns or sets the flag specifying whether or not to update the sketch during the builder commit. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SketchConstraintBuilderConstraint Enumeration | the types of the constraint |
Property Detail¶
Centerline¶
-
SketchConstraintBuilder.
Centerline
¶ Returns the centerline for a symmetric constraint type
-------------------------------------
Getter Method
Signature
Centerline
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
ConstraintType¶
-
SketchConstraintBuilder.
ConstraintType
¶ Returns or sets the constraint type
-------------------------------------
Getter Method
Signature
ConstraintType
Returns: Return type: NXOpen.SketchConstraintBuilderConstraint
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstraintType
Parameters: constraintType ( NXOpen.SketchConstraintBuilderConstraint
) –New in version NX8.5.0.
License requirements: None.
GeometryToConstrain¶
-
SketchConstraintBuilder.
GeometryToConstrain
¶ Returns the geometries to be constrained
-------------------------------------
Getter Method
Signature
GeometryToConstrain
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX8.5.0.
License requirements: None.
GeometryToConstrainTo¶
-
SketchConstraintBuilder.
GeometryToConstrainTo
¶ Returns the secondary geometries to be constrained
-------------------------------------
Getter Method
Signature
GeometryToConstrainTo
Returns: Return type: NXOpen.SelectNXObject
New in version NX8.5.0.
License requirements: None.
MakeReference¶
-
SketchConstraintBuilder.
MakeReference
¶ Returns or sets the flag specifying whether or not to make the centerline reference geometry
-------------------------------------
Getter Method
Signature
MakeReference
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MakeReference
Parameters: makeReference (bool) – New in version NX8.5.0.
License requirements: None.
UpdateSketchAtCommit¶
-
SketchConstraintBuilder.
UpdateSketchAtCommit
¶ Returns or sets the flag specifying whether or not to update the sketch during the builder commit.
The default value is true. If the value is set to false, the sketch will not update during the builder commit.
-------------------------------------
Getter Method
Signature
UpdateSketchAtCommit
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpdateSketchAtCommit
Parameters: updateSketch (bool) – New in version NX11.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
SketchConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.