SketchAutoDimensionBuilder Class¶
-
class
NXOpen.
SketchAutoDimensionBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchAutoDimensionBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateAutoDimensionBuilder()
Default values.
Property Value DimensionType Automatic New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
DimensionType | Returns or sets the enum dim type |
SelectionObject | Returns the selected sketch curves to auto dimension |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetRules | Get the auto dimensioning rule list from builder |
SetRules | Set the auto dimensioning rule list to builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SketchAutoDimensionBuilderDimType Enumeration | dimension type to be created |
Property Detail¶
DimensionType¶
-
SketchAutoDimensionBuilder.
DimensionType
¶ Returns or sets the enum dim type
-------------------------------------
Getter Method
Signature
DimensionType
Returns: Return type: NXOpen.SketchAutoDimensionBuilderDimType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DimensionType
Parameters: dimensionType ( NXOpen.SketchAutoDimensionBuilderDimType
) –New in version NX7.5.0.
License requirements: None.
SelectionObject¶
-
SketchAutoDimensionBuilder.
SelectionObject
¶ Returns the selected sketch curves to auto dimension
-------------------------------------
Getter Method
Signature
SelectionObject
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
Method Detail¶
GetRules¶
-
SketchAutoDimensionBuilder.
GetRules
¶ Get the auto dimensioning rule list from builder
Signature
GetRules()
Returns: Auto Dimension Rules Return type: list of NXOpen.SketchAutoDimensioningRule
New in version NX7.5.0.
License requirements: None.
SetRules¶
-
SketchAutoDimensionBuilder.
SetRules
¶ Set the auto dimensioning rule list to builder.
All the rules are expected to be in the list exactly once. Variable count can not be zero or negative.
Signature
SetRules(rules)
Parameters: rules (list of NXOpen.SketchAutoDimensioningRule
) – Auto Dimension RulesNew in version NX7.5.0.
License requirements: None.
Validate¶
-
SketchAutoDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.