SketchAssociativeTrimBuilder Class¶
-
class
NXOpen.
SketchAssociativeTrimBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.SketchAssociativeTrimBuilder
To create a new instance of this class, use
NXOpen.SketchCollection.CreateSketchAssociativeTrimBuilder()
Default values.
Property Value TrimType Keep New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
RecipeCurves | Returns the input curves. |
Tag | Returns the Tag for this object. |
TrimType | Returns or sets the trim region type - if the region needs to be kept/discarded |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateSection | The function creates a new empty section object and adds it to the builder |
DeselectRegion | The region corresponding to help point will be delsected from being kept/discarded depending on trim type |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetSections | This function gets all sections of the trim constraint during create/edit |
RemoveSection | The function removes the given section from the builder |
ResetRegions | The regions are forced to be deselected |
SelectRegion | The function sets help point for region select. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateRegions | The regions are recreated and updated to reflect the change in the boundary curves |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SketchAssociativeTrimBuilderTrimOption Enumeration | Represents the keep discard options for selected region |
Property Detail¶
RecipeCurves¶
-
SketchAssociativeTrimBuilder.
RecipeCurves
¶ Returns the input curves.
These curves must be a part of a single continuous recipe chain.
-------------------------------------
Getter Method
Signature
RecipeCurves
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX6.0.0.
License requirements: None.
TrimType¶
-
SketchAssociativeTrimBuilder.
TrimType
¶ Returns or sets the trim region type - if the region needs to be kept/discarded
-------------------------------------
Getter Method
Signature
TrimType
Returns: Return type: NXOpen.SketchAssociativeTrimBuilderTrimOption
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TrimType
Parameters: option ( NXOpen.SketchAssociativeTrimBuilderTrimOption
) –New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Method Detail¶
CreateSection¶
-
SketchAssociativeTrimBuilder.
CreateSection
¶ The function creates a new empty section object and adds it to the builder
Signature
CreateSection()
Returns: New section object Return type: NXOpen.Section
New in version NX6.0.0.
License requirements: None.
DeselectRegion¶
-
SketchAssociativeTrimBuilder.
DeselectRegion
¶ The region corresponding to help point will be delsected from being kept/discarded depending on trim type
Signature
DeselectRegion(helpPoint)
Parameters: helpPoint ( NXOpen.Point3d
) – Help point for region selectionNew in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
GetSections¶
-
SketchAssociativeTrimBuilder.
GetSections
¶ This function gets all sections of the trim constraint during create/edit
Signature
GetSections()
Returns: All the sections associated with the builder Return type: list of NXOpen.Section
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
RemoveSection¶
-
SketchAssociativeTrimBuilder.
RemoveSection
¶ The function removes the given section from the builder
Signature
RemoveSection(section)
Parameters: section ( NXOpen.Section
) – Section object to removeNew in version NX6.0.0.
License requirements: None.
ResetRegions¶
-
SketchAssociativeTrimBuilder.
ResetRegions
¶ The regions are forced to be deselected
Signature
ResetRegions()
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SelectRegion¶
-
SketchAssociativeTrimBuilder.
SelectRegion
¶ The function sets help point for region select.
The region corresponding to help point will be kept/discarded depending on trim type
Signature
SelectRegion(helpPoint)
Parameters: helpPoint ( NXOpen.Point3d
) – Help point for region selectionNew in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
UpdateRegions¶
-
SketchAssociativeTrimBuilder.
UpdateRegions
¶ The regions are recreated and updated to reflect the change in the boundary curves
Signature
UpdateRegions()
New in version NX6.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
SketchAssociativeTrimBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.