StiffenerBuilder Class¶
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Features.ShipDesign.Stiffener
builderTo create a new instance of this class, use
NXOpen.Features.ShipCollection.CreateStiffenerBuilder()
Default values.
Property Value AddNeatTrim 0 AngularTolerance 0.5 AttachmentPlateOption Inferred DistanceTolerance 0.0254 EdgeReinforcementAlignment Center EndCutType None EndEndCut.ConnectionType Connected EndEndCut.DraftAngle.Value 0 EndEndCut.DraftOffset.Value 0 (millimeters part), 0 (inches part) EndEndCut.DraftType Trim EndEndCut.LimitType Value EndEndCut.Offset.Value 0 (millimeters part), 0 (inches part) EndEndCut.SelectionType FacesWithAttributes EndEndCut.ShearAngle.Value 0 EndEndCut.TiltAngle.Value 0 EndLimit.LimitMethod Value EndLimit.LimitValue.Value 0 FaceOffset.Value 0 (millimeters part), 0 (inches part) IncludeRelief 1 KnuckleOption None MountingAngle.Value 0 MountingMethod NoOffset OrientType FaceNormal OrientationAngleRule RightHand OrientationDefinitionBuilder.MeasureAngles NormaltoCurve OrientationDefinitionBuilder.ShowSurfaceAngles 0 OrientationDefinitionBuilder.ShowTwistRate 0 OrientationDefinitionBuilder.ShowWebAngles 0 PathOffset.Value 0 (millimeters part), 0 (inches part) StiffenerBySupportPathData.LengthParams.Value 300 (millimeters part), 100 (inches part) StiffenerBySupportPathData.OrientationBySupport 0 StockData.AnchorPoint 0 StockData.PlateHeight.Value 50 (millimeters part), 2 (inches part) StockData.PlateStockData.KnuckleRatio 3.0 StockData.PlateStockData.KnuckleSmoothAngle 3.0 StockData.PlateStockData.MaterialOption 0 StockData.PlateStockData.OppositeThickness.Value 0 (millimeters part), 0 (inches part) StockData.PlateStockData.RestrictThicknessToMaterial true StockData.PlateStockData.ThickenOption SingleSided StockData.PlateStockData.Thickness.Value 10 (millimeters part), 0.5 (inches part) StockData.PlateStockData.ThicknessSourceOption List StockData.SectionType Profile New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
AddNeatTrim | Returns or sets the option to add neat trim to plate edge reinforcements. |
AdoptionAnchorPointList | Returns the adoption anchor point list. |
AdoptionBaseFaces | Returns the adoption base faces. |
AdoptionBodies | Returns the adoption bodies, which are used to create multiple adoption stiffeners. |
AdoptionEndCutFaces1 | Returns the adoption end cut 1 faces. |
AdoptionEndCutFaces2 | Returns the adoption end cut 2 faces. |
AdoptionMoldFaces | Returns the adoption mold faces. |
AdoptionOpposingMoldFaces | Returns the adoption opposing mold faces. |
AdoptionTopFaces | Returns the adoption top faces. |
AngularTolerance | Returns or sets the angular tolerance (degrees) |
ApplyFlangeSetback | Returns or sets the flange set back option for stiffener by support, which indicates if the flange set back should be applied or not |
ApplyWebSetback | Returns or sets the web set back option for stiffener by support, which indicates if the web set back should be applied or not |
AttachmentPlate | Returns the selected attachment plate |
AttachmentPlateOption | Returns or sets the attachment plate option |
ConnectAngle | Returns or sets the connect angle of stiffener by support in degrees, negative value is not allowed |
DistanceTolerance | Returns or sets the distance tolerance (part units) |
EdgeReinforcementAlignment | Returns or sets the edge reinforcement alignment |
EdgeReinforcementPlacementMethod | Returns or sets the edge reinforcement placement method |
EndCutType | Returns or sets the number of end cuts to apply |
EndEndCut | Returns the end end cut |
EndLimit | Returns the end path limit |
FaceOffset | Returns the face offset expression |
FaceReverseDirection | Returns or sets the face reverse direction flag |
IncludeRelief | Returns or sets the include relief option |
KnuckleOption | Returns or sets the stiffener knuckle option |
MountingAngle | Returns the mounting angle expression |
MountingMethod | Returns or sets the mounting method |
OrientCsys | Returns the orientation coordinate systems (when OrientType is DatumCSys |
OrientType | Returns or sets the stiffener orientation type |
OrientVector | Returns or sets the orientation vector (when OrientType is Vector) |
OrientationAngleRule | Returns or sets the angle rule to use when measuring angles. |
OrientationDefinitionBuilder | Returns the builder used to define the orientation for the stiffener. |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PathGeometry | Returns the path geometry |
PathOffset | Returns the path offset expression |
PathReverseDirection | Returns or sets the path reverse direction flag |
PlacementGeometry | Returns the placement geometry |
ReferenceDirection | Returns or sets the reference direction |
ReferencePoint | Returns or sets the reference point (part units) |
ShipNames | Returns the ship name builder. |
StartEndCut | Returns the start end cut |
StartLimit | Returns the start path limit |
StiffenerBySupportPathData | Returns the path data used to define the support information of the stiffener. |
StockData | Returns the stock data |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Type | Returns or sets the feature type: Stiffener or Edge Reinforcement |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
CreatePath | Creates path curves for use by the orientation definition object |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DestroyPath | Destroy the path curves |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
GetShowMigratedBody | Gets the show migrated body flag. |
GetStiffenerBySupportBoundaryAttachedPlate | Returns the plate body where the stiffener by support boundary is attached. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetShowMigratedBody | Sets the show migrated body flag. |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
StiffenerBuilderAttachmentOption Enumeration | The stiffener attachment plate option |
StiffenerBuilderEdgeReinforcementAlignmentMethod Enumeration | the edge reinforcement alignment method |
StiffenerBuilderEdgeReinforcementPlacementMethods Enumeration | The edge reinforcement placement method |
StiffenerBuilderEndCutTypes Enumeration | this specifies how the end cuts are applied |
StiffenerBuilderKnuckleOptions Enumeration | the knuckle option |
StiffenerBuilderMountingMethods Enumeration | the mounting method offset type |
StiffenerBuilderOrientationMethod Enumeration | The stiffener orientation method |
StiffenerBuilderTypes Enumeration | the feature type: Stiffener or Edge Reinforcement |
Property Detail¶
AddNeatTrim¶
-
StiffenerBuilder.
AddNeatTrim
¶ Returns or sets the option to add neat trim to plate edge reinforcements.
Note this only applies to plates.
-------------------------------------
Getter Method
Signature
AddNeatTrim
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AddNeatTrim
Parameters: addNeatTrim (bool) – New in version NX11.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
AdoptionAnchorPointList¶
-
StiffenerBuilder.
AdoptionAnchorPointList
¶ Returns the adoption anchor point list.
-------------------------------------
Getter Method
Signature
AdoptionAnchorPointList
Returns: Return type: NXOpen.NXObjectList
New in version NX8.5.0.
License requirements: None.
AdoptionBaseFaces¶
-
StiffenerBuilder.
AdoptionBaseFaces
¶ Returns the adoption base faces.
-------------------------------------
Getter Method
Signature
AdoptionBaseFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AdoptionBodies¶
-
StiffenerBuilder.
AdoptionBodies
¶ Returns the adoption bodies, which are used to create multiple adoption stiffeners.
-------------------------------------
Getter Method
Signature
AdoptionBodies
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
AdoptionEndCutFaces1¶
-
StiffenerBuilder.
AdoptionEndCutFaces1
¶ Returns the adoption end cut 1 faces.
-------------------------------------
Getter Method
Signature
AdoptionEndCutFaces1
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AdoptionEndCutFaces2¶
-
StiffenerBuilder.
AdoptionEndCutFaces2
¶ Returns the adoption end cut 2 faces.
-------------------------------------
Getter Method
Signature
AdoptionEndCutFaces2
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AdoptionMoldFaces¶
-
StiffenerBuilder.
AdoptionMoldFaces
¶ Returns the adoption mold faces.
-------------------------------------
Getter Method
Signature
AdoptionMoldFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AdoptionOpposingMoldFaces¶
-
StiffenerBuilder.
AdoptionOpposingMoldFaces
¶ Returns the adoption opposing mold faces.
-------------------------------------
Getter Method
Signature
AdoptionOpposingMoldFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AdoptionTopFaces¶
-
StiffenerBuilder.
AdoptionTopFaces
¶ Returns the adoption top faces.
-------------------------------------
Getter Method
Signature
AdoptionTopFaces
Returns: Return type: NXOpen.ScCollector
New in version NX8.5.0.
License requirements: None.
AngularTolerance¶
-
StiffenerBuilder.
AngularTolerance
¶ Returns or sets the angular tolerance (degrees)
-------------------------------------
Getter Method
Signature
AngularTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AngularTolerance
Parameters: angularTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ApplyFlangeSetback¶
-
StiffenerBuilder.
ApplyFlangeSetback
¶ Returns or sets the flange set back option for stiffener by support, which indicates if the flange set back should be applied or not
-------------------------------------
Getter Method
Signature
ApplyFlangeSetback
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyFlangeSetback
Parameters: applyFlangeSetback (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ApplyWebSetback¶
-
StiffenerBuilder.
ApplyWebSetback
¶ Returns or sets the web set back option for stiffener by support, which indicates if the web set back should be applied or not
-------------------------------------
Getter Method
Signature
ApplyWebSetback
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplyWebSetback
Parameters: applyWebSetback (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
AttachmentPlate¶
-
StiffenerBuilder.
AttachmentPlate
¶ Returns the selected attachment plate
-------------------------------------
Getter Method
Signature
AttachmentPlate
Returns: Return type: NXOpen.SelectDisplayableObject
New in version NX9.0.0.
License requirements: None.
AttachmentPlateOption¶
-
StiffenerBuilder.
AttachmentPlateOption
¶ Returns or sets the attachment plate option
-------------------------------------
Getter Method
Signature
AttachmentPlateOption
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderAttachmentOption
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AttachmentPlateOption
Parameters: attachmentPlateOption ( NXOpen.Features.ShipDesign.StiffenerBuilderAttachmentOption
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ConnectAngle¶
-
StiffenerBuilder.
ConnectAngle
¶ Returns or sets the connect angle of stiffener by support in degrees, negative value is not allowed
-------------------------------------
Getter Method
Signature
ConnectAngle
Returns: Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConnectAngle
Parameters: connectAngle (float) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
DistanceTolerance¶
-
StiffenerBuilder.
DistanceTolerance
¶ Returns or sets the distance tolerance (part units)
-------------------------------------
Getter Method
Signature
DistanceTolerance
Returns: Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceTolerance
Parameters: distanceTolerance (float) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
EdgeReinforcementAlignment¶
-
StiffenerBuilder.
EdgeReinforcementAlignment
¶ Returns or sets the edge reinforcement alignment
-------------------------------------
Getter Method
Signature
EdgeReinforcementAlignment
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderEdgeReinforcementAlignmentMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeReinforcementAlignment
Parameters: edgeReinforcementAlignment ( NXOpen.Features.ShipDesign.StiffenerBuilderEdgeReinforcementAlignmentMethod
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
EdgeReinforcementPlacementMethod¶
-
StiffenerBuilder.
EdgeReinforcementPlacementMethod
¶ Returns or sets the edge reinforcement placement method
-------------------------------------
Getter Method
Signature
EdgeReinforcementPlacementMethod
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderEdgeReinforcementPlacementMethods
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EdgeReinforcementPlacementMethod
Parameters: edgeReinforcementPlacementMethod ( NXOpen.Features.ShipDesign.StiffenerBuilderEdgeReinforcementPlacementMethods
) –New in version NX10.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
EndCutType¶
-
StiffenerBuilder.
EndCutType
¶ Returns or sets the number of end cuts to apply
-------------------------------------
Getter Method
Signature
EndCutType
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderEndCutTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndCutType
Parameters: endcutType ( NXOpen.Features.ShipDesign.StiffenerBuilderEndCutTypes
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
EndEndCut¶
-
StiffenerBuilder.
EndEndCut
¶ Returns the end end cut
-------------------------------------
Getter Method
Signature
EndEndCut
Returns: Return type: NXOpen.Features.ShipDesign.EndCutBuilder
New in version NX8.0.0.
License requirements: None.
EndLimit¶
-
StiffenerBuilder.
EndLimit
¶ Returns the end path limit
-------------------------------------
Getter Method
Signature
EndLimit
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerLimitBuilder
New in version NX8.0.0.
License requirements: None.
FaceOffset¶
-
StiffenerBuilder.
FaceOffset
¶ Returns the face offset expression
-------------------------------------
Getter Method
Signature
FaceOffset
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
FaceReverseDirection¶
-
StiffenerBuilder.
FaceReverseDirection
¶ Returns or sets the face reverse direction flag
-------------------------------------
Getter Method
Signature
FaceReverseDirection
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FaceReverseDirection
Parameters: faceReverseDirection (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
IncludeRelief¶
-
StiffenerBuilder.
IncludeRelief
¶ Returns or sets the include relief option
-------------------------------------
Getter Method
Signature
IncludeRelief
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IncludeRelief
Parameters: includeRelief (bool) – New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
KnuckleOption¶
-
StiffenerBuilder.
KnuckleOption
¶ Returns or sets the stiffener knuckle option
-------------------------------------
Getter Method
Signature
KnuckleOption
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderKnuckleOptions
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
KnuckleOption
Parameters: knuckleOption ( NXOpen.Features.ShipDesign.StiffenerBuilderKnuckleOptions
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
MountingAngle¶
-
StiffenerBuilder.
MountingAngle
¶ Returns the mounting angle expression
-------------------------------------
Getter Method
Signature
MountingAngle
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
MountingMethod¶
-
StiffenerBuilder.
MountingMethod
¶ Returns or sets the mounting method
-------------------------------------
Getter Method
Signature
MountingMethod
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderMountingMethods
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MountingMethod
Parameters: mountingMethod ( NXOpen.Features.ShipDesign.StiffenerBuilderMountingMethods
) –New in version NX8.0.0.
License requirements: nx_ship_concept (“Ship Concept”)
OrientCsys¶
-
StiffenerBuilder.
OrientCsys
¶ Returns the orientation coordinate systems (when OrientType is DatumCSys
-------------------------------------
Getter Method
Signature
OrientCsys
Returns: Return type: NXOpen.Features.SelectDatumCsysList
New in version NX8.0.0.
License requirements: None.
OrientType¶
-
StiffenerBuilder.
OrientType
¶ Returns or sets the stiffener orientation type
-------------------------------------
Getter Method
Signature
OrientType
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderOrientationMethod
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientType
Parameters: orientType ( NXOpen.Features.ShipDesign.StiffenerBuilderOrientationMethod
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
OrientVector¶
-
StiffenerBuilder.
OrientVector
¶ Returns or sets the orientation vector (when OrientType is Vector)
-------------------------------------
Getter Method
Signature
OrientVector
Returns: Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientVector
Parameters: orientVector ( NXOpen.Direction
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
OrientationAngleRule¶
-
StiffenerBuilder.
OrientationAngleRule
¶ Returns or sets the angle rule to use when measuring angles.
-------------------------------------
Getter Method
Signature
OrientationAngleRule
Returns: Return type: NXOpen.Features.ShipDesign.FeatureParmsBuilderOrientationAngleRuleTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OrientationAngleRule
Parameters: angleRule ( NXOpen.Features.ShipDesign.FeatureParmsBuilderOrientationAngleRuleTypes
) –New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
OrientationDefinitionBuilder¶
-
StiffenerBuilder.
OrientationDefinitionBuilder
¶ Returns the builder used to define the orientation for the stiffener.
-------------------------------------
Getter Method
Signature
OrientationDefinitionBuilder
Returns: Return type: NXOpen.Features.ShipDesign.OrientationDefinitionBuilder
New in version NX9.0.0.
License requirements: None.
PathGeometry¶
-
StiffenerBuilder.
PathGeometry
¶ Returns the path geometry
-------------------------------------
Getter Method
Signature
PathGeometry
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.0.0.
License requirements: None.
PathOffset¶
-
StiffenerBuilder.
PathOffset
¶ Returns the path offset expression
-------------------------------------
Getter Method
Signature
PathOffset
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
PathReverseDirection¶
-
StiffenerBuilder.
PathReverseDirection
¶ Returns or sets the path reverse direction flag
-------------------------------------
Getter Method
Signature
PathReverseDirection
Returns: Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathReverseDirection
Parameters: pathReverseDirection (bool) – New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
PlacementGeometry¶
-
StiffenerBuilder.
PlacementGeometry
¶ Returns the placement geometry
-------------------------------------
Getter Method
Signature
PlacementGeometry
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX8.0.0.
License requirements: None.
ReferenceDirection¶
-
StiffenerBuilder.
ReferenceDirection
¶ Returns or sets the reference direction
-------------------------------------
Getter Method
Signature
ReferenceDirection
Returns: Return type: NXOpen.Vector3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferenceDirection
Parameters: referenceDirection ( NXOpen.Vector3d
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ReferencePoint¶
-
StiffenerBuilder.
ReferencePoint
¶ Returns or sets the reference point (part units)
-------------------------------------
Getter Method
Signature
ReferencePoint
Returns: Return type: NXOpen.Point3d
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReferencePoint
Parameters: referencePoint ( NXOpen.Point3d
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
ShipNames¶
-
StiffenerBuilder.
ShipNames
¶ Returns the ship name builder.
The ship name builder is used to construct the part name of the structure.
-------------------------------------
Getter Method
Signature
ShipNames
Returns: Return type: NXOpen.Features.ShipDesign.ShipNamesBuilder
New in version NX11.0.0.
License requirements: None.
StartEndCut¶
-
StiffenerBuilder.
StartEndCut
¶ Returns the start end cut
-------------------------------------
Getter Method
Signature
StartEndCut
Returns: Return type: NXOpen.Features.ShipDesign.EndCutBuilder
New in version NX8.0.0.
License requirements: None.
StartLimit¶
-
StiffenerBuilder.
StartLimit
¶ Returns the start path limit
-------------------------------------
Getter Method
Signature
StartLimit
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerLimitBuilder
New in version NX8.0.0.
License requirements: None.
StiffenerBySupportPathData¶
-
StiffenerBuilder.
StiffenerBySupportPathData
¶ Returns the path data used to define the support information of the stiffener.
-------------------------------------
Getter Method
Signature
StiffenerBySupportPathData
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBySupportPathBuilder
New in version NX9.0.0.
License requirements: None.
StockData¶
-
StiffenerBuilder.
StockData
¶ Returns the stock data
-------------------------------------
Getter Method
Signature
StockData
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerStockBuilder
New in version NX8.0.0.
License requirements: None.
Type¶
-
StiffenerBuilder.
Type
¶ Returns or sets the feature type: Stiffener or Edge Reinforcement
-------------------------------------
Getter Method
Signature
Type
Returns: Return type: NXOpen.Features.ShipDesign.StiffenerBuilderTypes
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type
Parameters: type ( NXOpen.Features.ShipDesign.StiffenerBuilderTypes
) –New in version NX8.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
Method Detail¶
CreatePath¶
-
StiffenerBuilder.
CreatePath
¶ Creates path curves for use by the orientation definition object
Signature
CreatePath()
Returns: a tuple Return type: A tuple consisting of (curves, faces). curves is a list of NXOpen.NXObject
. The curves defining the path of the profile that is being oriented. faces is a list ofNXOpen.DisplayableObject
. The faces/datums defining the placement of the profile that is being oriented.New in version NX9.0.0.
License requirements: None.
DestroyPath¶
-
StiffenerBuilder.
DestroyPath
¶ Destroy the path curves
Signature
DestroyPath(curves)
Parameters: curves (list of NXOpen.NXObject
) – The curves defining the path of the profile that is being oriented.New in version NX9.0.0.
License requirements: nx_ship_detail (“Ship Detail Design”)
GetShowMigratedBody¶
-
StiffenerBuilder.
GetShowMigratedBody
¶ Gets the show migrated body flag.
Reserved for administrator use only.
Signature
GetShowMigratedBody()
Returns: Return type: bool New in version NX8.5.3.
License requirements: None.
GetStiffenerBySupportBoundaryAttachedPlate¶
-
StiffenerBuilder.
GetStiffenerBySupportBoundaryAttachedPlate
¶ Returns the plate body where the stiffener by support boundary is attached.
Signature
GetStiffenerBySupportBoundaryAttachedPlate(boundary)
Parameters: boundary ( NXOpen.Body
) –Returns: Return type: NXOpen.Body
New in version NX11.0.1.
License requirements: nx_ship_detail (“Ship Detail Design”)
SetShowMigratedBody¶
-
StiffenerBuilder.
SetShowMigratedBody
¶ Sets the show migrated body flag.
Reserved for administrator use only.
Signature
SetShowMigratedBody(showMigratedBody)
Parameters: showMigratedBody (bool) – New in version NX8.5.3.
License requirements: nx_ship_detail (“Ship Detail Design”)
Validate¶
-
StiffenerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.