StiffenerBuilderTypes Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBuilder.Types is an alias for NXOpen.Features.ShipDesign.StiffenerBuilderTypes
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilderTypes
¶ Bases:
object
the feature type: Stiffener or Edge Reinforcement
Enum Members
Enum Member Enum Member Description Stiffener Stiffener type EdgeReinforcement Edge Reinforcement type AdoptStiffener Adoption Stiffener type AdoptEdgeReinforcement Adoption Edge Reinforcement type StiffenerBySupport Stiffener By Support type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-