StiffenerBuilderOrientationMethod Enumeration¶
NXOpen.Features.ShipDesign.StiffenerBuilder.OrientationMethod is an alias for NXOpen.Features.ShipDesign.StiffenerBuilderOrientationMethod
-
class
NXOpen.Features.ShipDesign.
StiffenerBuilderOrientationMethod
¶ Bases:
object
The stiffener orientation method
Enum Members
Enum Member Enum Member Description FaceNormal Align stiffener with face normal Vector Align stiffener with vector DatumCSYS Align stiffener with one or more coordinate systems -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-