DeformDefinitionBuilder Class¶
-
class
NXOpen.Features.
DeformDefinitionBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Used as a place holder for selected member features, expressions and external references for a deform definition feature record that is to be created.
To create a new instance of this class, use
NXOpen.Features.FeatureCollection.CreateDeformDefinitionBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetExpressionsData | Sets data of single expression for deform definition feature. |
SetExternalReferences | Sets external references for deform definition feature. |
SetHelpUrl | Sets help url on deform definition feature. |
SetMemberFeatures | Sets the list of member feature records for deform definition feature. |
SetName | Sets name for deform definition feature. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DeformDefinitionBuilderExpressionType Enumeration | Specifies the way of providing input to expression during deform instantiation. |
DeformDefinitionBuilderRangeType Enumeration | Specifies type of range of input values when NXOpen.Features.DeformDefinitionBuilderExpressionType is NXOpen.Features.DeformDefinitionBuilderExpressionType.Range . |
Method Detail¶
SetExpressionsData¶
-
DeformDefinitionBuilder.
SetExpressionsData
¶ Sets data of single expression for deform definition feature.
For multiple expressions, this needs to be called multiple times.
Signature
SetExpressionsData(expData, defineValues)
Parameters: - expData (
NXOpen.Features.DeformDefinitionBuilderJaDeformDefinitionExpData_Struct
) – - defineValues (list of str) –
New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- expData (
SetExternalReferences¶
-
DeformDefinitionBuilder.
SetExternalReferences
¶ Sets external references for deform definition feature.
Signature
SetExternalReferences(extRefs, refPrompts)
Parameters: - extRefs (list of
NXOpen.DisplayableObject
) – - refPrompts (list of str) –
New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
- extRefs (list of
SetHelpUrl¶
-
DeformDefinitionBuilder.
SetHelpUrl
¶ Sets help url on deform definition feature.
Signature
SetHelpUrl(helpUrl)
Parameters: helpUrl (str) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetMemberFeatures¶
-
DeformDefinitionBuilder.
SetMemberFeatures
¶ Sets the list of member feature records for deform definition feature.
Signature
SetMemberFeatures(memberFrecs)
Parameters: memberFrecs (list of NXOpen.Features.Feature
) –New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
SetName¶
-
DeformDefinitionBuilder.
SetName
¶ Sets name for deform definition feature.
Signature
SetName(name)
Parameters: name (str) – New in version NX12.0.0.
License requirements: solid_modeling (“SOLIDS MODELING”)
Validate¶
-
DeformDefinitionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.