DeformDefinitionBuilderExpressionType Enumeration¶
NXOpen.Features.DeformDefinitionBuilder.ExpressionType is an alias for NXOpen.Features.DeformDefinitionBuilderExpressionType
-
class
NXOpen.Features.
DeformDefinitionBuilderExpressionType
¶ Bases:
object
Specifies the way of providing input to expression during deform instantiation.
Enum Members
Enum Member Enum Member Description Exp Regular expression. Input can be any value. Range Input is within a range of values (integer or double) Option Input is from a set of fixed values. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-