DeformDefinitionBuilderRangeType Enumeration¶
NXOpen.Features.DeformDefinitionBuilder.RangeType is an alias for NXOpen.Features.DeformDefinitionBuilderRangeType
-
class
NXOpen.Features.
DeformDefinitionBuilderRangeType
¶ Bases:
object
Specifies type of range of input values when
NXOpen.Features.DeformDefinitionBuilderExpressionType
isNXOpen.Features.DeformDefinitionBuilderExpressionType.Range
.Enum Members
Enum Member Enum Member Description Int Range of integer numbers. Real Range of fractional numbers. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-