DeformDefinitionBuilderJaDeformDefinitionExpData_Struct Struct¶
NXOpen.Features.DeformDefinitionBuilder.JaDeformDefinitionExpData is an alias for NXOpen.Features.DeformDefinitionBuilderJaDeformDefinitionExpData_Struct
-
class
NXOpen.Features.
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct
¶ Bases:
object
.
Constructor: NXOpen.Features.DeformDefinitionBuilder.JaDeformDefinitionExpData()
Fields¶
Field | Description |
---|---|
Type | One of the NXOpen.Features.DeformDefinitionBuilderExpressionType values. |
Exp | Tag of NXOpen.Expression object. |
ExpName | Name of expression. |
LowEnd | Minimum value in range of input values for expression. |
HighEnd | Maximum value in range of input values for expression. |
ScaleType | One of the NXOpen.Features.DeformDefinitionBuilderRangeType values when type is NXOpen.Features.DeformDefinitionBuilderExpressionType.Range . |
Type¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
Type
¶ One of the
NXOpen.Features.DeformDefinitionBuilderExpressionType
values.-------------------------------------
Field Value Type:int
Exp¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
Exp
¶ Tag of
NXOpen.Expression
object.-------------------------------------
Field Value Type:
NXOpen.Expression
ExpName¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
ExpName
¶ Name of expression.
This will be displayed in UI.
-------------------------------------
Field Value Type:str
LowEnd¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
LowEnd
¶ Minimum value in range of input values for expression.
-------------------------------------
Field Value Type:str
HighEnd¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
HighEnd
¶ Maximum value in range of input values for expression.
-------------------------------------
Field Value Type:str
ScaleType¶
-
DeformDefinitionBuilderJaDeformDefinitionExpData_Struct.
ScaleType
¶ One of the
NXOpen.Features.DeformDefinitionBuilderRangeType
values when type isNXOpen.Features.DeformDefinitionBuilderExpressionType.Range
.-------------------------------------
Field Value Type:int