NcmPlanarBuilder Class¶
-
class
NXOpen.CAM.
NcmPlanarBuilder
¶ Bases:
NXOpen.CAM.NcmSubopBuilder
Represents a
NXOpen.CAM.NcmPlanarBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ApplySafetyToDirect | Returns or sets the apply safety to direct value |
ClearanceBuilder | Returns the clearance builder (inheritable tool dep) |
CollisionCheck | Returns or sets the collision check activation |
CutcomMinimumAngle | Returns or sets the cutter compensation minimum angle |
CutcomMinimumMoveBuilder | Returns the cutter compensation minimum move builder (inheritable tool dep) |
CutcomOutputContactPoint | Returns or sets the cutter compensation output contact point status |
CutcomOutputPlane | Returns or sets the cutter compensation output plane status |
CutcomTrackingPointType | Returns or sets the cutter compensation tracking point selection |
CutcomType | Returns or sets the cutter compensation type |
DefaultRegionStartType | Returns or sets the region start type |
EngageClosedAreaBuilder | Returns the default engage closed area builder |
EngageInitialClosedBuilder | Returns the initial engage closed area builder |
EngageInitialOpenBuilder | Returns the initial engage open area builder |
EngageOpenAreaBuilder | Returns the default engage open area builder |
FinalSafeDistanceBuilder | Returns the final safe distance builder (inheritable tool dep) |
FinalType | Returns or sets the final type |
InitialSafeDistanceBuilder | Returns the initial safe distance builder (inheritable tool dep) |
InitialType | Returns or sets the initial type |
LimitEngRetToCutRegion | Returns or sets the flag to control limitation of engage and retract motions to cut regions |
OverlapDistanceBuilder | Returns the start/drill points overlap distance builder (inheritable tool dep) |
PredrillPointsEffectDistBuilder | Returns the pre-drill points effective distance builder (inheritable tool dep) |
PredrillPointsOutput | Returns or sets the pre-drill points output option |
PredrillPointsUseEffectDist | Returns or sets the pre-drill points use effective distance |
RetractAreaBuilder | Returns the retract area builder |
RetractFinalBuilder | Returns the final retract builder |
SmoothingBuilder | Returns the smoothing builder |
StartPointsEffectDistBuilder | Returns the region start points effective distance builder (inheritable tool dep) |
StartPointsUseEffectDist | Returns or sets the start points use effective distance |
SuppressCutcom | Returns or sets the suppress cutter compensation |
Tag | Returns the Tag for this object. |
TransferAvoidanceFromBuilder | Returns the from point builder |
TransferAvoidanceGohomeBuilder | Returns the gohome point builder |
TransferAvoidanceReturnBuilder | Returns the return point builder |
TransferAvoidanceStartBuilder | Returns the start point builder |
TransferBetweenLevelsSafeDistanceBuilder | Returns the transfer between levels safe distance builder (inheritable tool dep) |
TransferBetweenLevelsType | Returns or sets the transfer between levels type |
TransferBetweenRegionsBuilder | Returns the Transfer Between Regions builder |
TransferBetweenRegionsSafeDistanceBuilder | Returns the transfer between regions safe distance builder (inheritable tool dep) |
TransferBetweenRegionsType | Returns or sets the transfer between regions type |
TransferWithinLevelsHeightBuilder | Returns the transfer within levels height builder (inheritable tool dep) |
TransferWithinLevelsMaxFollowDistanceBuilder | Returns the transfer within levels max follow distance builder (inheritable tool dep) |
TransferWithinLevelsSafeDistanceBuilder | Returns the transfer within levels safe distance builder (inheritable tool dep) |
TransferWithinLevelsType | Returns or sets the transfer within levels type |
TransferWithinLevelsWith | Returns or sets the transfer within levels strategy |
Methods¶
Method | Description |
---|---|
GetCustomizableItemBuilder | Returns the customizable item builder for given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetPredrillPoints | The pre-drill points |
GetRegionStartPoints | Returns region start points |
SetPredrillPoints | The pre-drill points |
SetRegionStartPoints | Sets region start points |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
NcmPlanarBuilderCutcomTypes Enumeration | Available types for cutter compensation in planar milling |
NcmPlanarBuilderFinalRet Enumeration | Available strategies for final retract in planar milling |
NcmPlanarBuilderFinalTypes Enumeration | Available types for final clearance in planar milling |
NcmPlanarBuilderInitialEng Enumeration | Available strategies for initial engage in planar milling |
NcmPlanarBuilderInitialTypes Enumeration | Available types for initial clearance in planar milling |
NcmPlanarBuilderPredrillPointsOutputOptions Enumeration | Available options for output of pre-drill points in planar milling |
NcmPlanarBuilderTransferBetweenLevelsTypes Enumeration | Available types for transfer between levels in planar milling |
NcmPlanarBuilderTransferBetweenRegionsTypes Enumeration | Available types for transfer between regions in planar milling |
NcmPlanarBuilderTransferWithinLevelsTypes Enumeration | Available types for transfer within levels in planar milling |
NcmPlanarBuilderTransferWithinLevelsWiths Enumeration | Available strategies for transfer within levels in planar milling |
Property Detail¶
ApplySafetyToDirect¶
-
NcmPlanarBuilder.
ApplySafetyToDirect
¶ Returns or sets the apply safety to direct value
-------------------------------------
Getter Method
Signature
ApplySafetyToDirect
Returns: the apply safety value Return type: bool New in version NX9.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApplySafetyToDirect
Parameters: applySafety (bool) – the apply safety value New in version NX9.0.3.
License requirements: cam_base (“CAM BASE”)
ClearanceBuilder¶
-
NcmPlanarBuilder.
ClearanceBuilder
¶ Returns the clearance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
ClearanceBuilder
Returns: Clearance Return type: NXOpen.CAM.NcmClearanceBuilder
New in version NX5.0.0.
License requirements: None.
CollisionCheck¶
-
NcmPlanarBuilder.
CollisionCheck
¶ Returns or sets the collision check activation
-------------------------------------
Getter Method
Signature
CollisionCheck
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CollisionCheck
Parameters: newValue (bool) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutcomMinimumAngle¶
-
NcmPlanarBuilder.
CutcomMinimumAngle
¶ Returns or sets the cutter compensation minimum angle
-------------------------------------
Getter Method
Signature
CutcomMinimumAngle
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutcomMinimumAngle
Parameters: minimumAngle (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutcomMinimumMoveBuilder¶
-
NcmPlanarBuilder.
CutcomMinimumMoveBuilder
¶ Returns the cutter compensation minimum move builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
CutcomMinimumMoveBuilder
Returns: The cutcom minimum move builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
CutcomOutputContactPoint¶
-
NcmPlanarBuilder.
CutcomOutputContactPoint
¶ Returns or sets the cutter compensation output contact point status
-------------------------------------
Getter Method
Signature
CutcomOutputContactPoint
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutcomOutputContactPoint
Parameters: newValue (bool) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutcomOutputPlane¶
-
NcmPlanarBuilder.
CutcomOutputPlane
¶ Returns or sets the cutter compensation output plane status
-------------------------------------
Getter Method
Signature
CutcomOutputPlane
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutcomOutputPlane
Parameters: outputPlane (bool) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutcomTrackingPointType¶
-
NcmPlanarBuilder.
CutcomTrackingPointType
¶ Returns or sets the cutter compensation tracking point selection
-------------------------------------
Getter Method
Signature
CutcomTrackingPointType
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutcomTrackingPointType
Parameters: newValue (int) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
CutcomType¶
-
NcmPlanarBuilder.
CutcomType
¶ Returns or sets the cutter compensation type
-------------------------------------
Getter Method
Signature
CutcomType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderCutcomTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutcomType
Parameters: cutcomType ( NXOpen.CAM.NcmPlanarBuilderCutcomTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
EngageClosedAreaBuilder¶
-
NcmPlanarBuilder.
EngageClosedAreaBuilder
¶ Returns the default engage closed area builder
-------------------------------------
Getter Method
Signature
EngageClosedAreaBuilder
Returns: the default engage closed area builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
EngageInitialClosedBuilder¶
-
NcmPlanarBuilder.
EngageInitialClosedBuilder
¶ Returns the initial engage closed area builder
-------------------------------------
Getter Method
Signature
EngageInitialClosedBuilder
Returns: the initial engage closed area builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
EngageInitialOpenBuilder¶
-
NcmPlanarBuilder.
EngageInitialOpenBuilder
¶ Returns the initial engage open area builder
-------------------------------------
Getter Method
Signature
EngageInitialOpenBuilder
Returns: the initial engage open area builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
EngageOpenAreaBuilder¶
-
NcmPlanarBuilder.
EngageOpenAreaBuilder
¶ Returns the default engage open area builder
-------------------------------------
Getter Method
Signature
EngageOpenAreaBuilder
Returns: the default engage open area builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
FinalSafeDistanceBuilder¶
-
NcmPlanarBuilder.
FinalSafeDistanceBuilder
¶ Returns the final safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
FinalSafeDistanceBuilder
Returns: The final safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
FinalType¶
-
NcmPlanarBuilder.
FinalType
¶ Returns or sets the final type
-------------------------------------
Getter Method
Signature
FinalType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderFinalTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinalType
Parameters: finalType ( NXOpen.CAM.NcmPlanarBuilderFinalTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
InitialSafeDistanceBuilder¶
-
NcmPlanarBuilder.
InitialSafeDistanceBuilder
¶ Returns the initial safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
InitialSafeDistanceBuilder
Returns: The initial safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
InitialType¶
-
NcmPlanarBuilder.
InitialType
¶ Returns or sets the initial type
-------------------------------------
Getter Method
Signature
InitialType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderInitialTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InitialType
Parameters: initialType ( NXOpen.CAM.NcmPlanarBuilderInitialTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
LimitEngRetToCutRegion¶
-
NcmPlanarBuilder.
LimitEngRetToCutRegion
¶ Returns or sets the flag to control limitation of engage and retract motions to cut regions
-------------------------------------
Getter Method
Signature
LimitEngRetToCutRegion
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LimitEngRetToCutRegion
Parameters: newValue (bool) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
OverlapDistanceBuilder¶
-
NcmPlanarBuilder.
OverlapDistanceBuilder
¶ Returns the start/drill points overlap distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
OverlapDistanceBuilder
Returns: The overlap distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
PredrillPointsEffectDistBuilder¶
-
NcmPlanarBuilder.
PredrillPointsEffectDistBuilder
¶ Returns the pre-drill points effective distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
PredrillPointsEffectDistBuilder
Returns: The predrill points effective distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
PredrillPointsOutput¶
-
NcmPlanarBuilder.
PredrillPointsOutput
¶ Returns or sets the pre-drill points output option
-------------------------------------
Getter Method
Signature
PredrillPointsOutput
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderPredrillPointsOutputOptions
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PredrillPointsOutput
Parameters: newValue ( NXOpen.CAM.NcmPlanarBuilderPredrillPointsOutputOptions
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
PredrillPointsUseEffectDist¶
-
NcmPlanarBuilder.
PredrillPointsUseEffectDist
¶ Returns or sets the pre-drill points use effective distance
-------------------------------------
Getter Method
Signature
PredrillPointsUseEffectDist
Returns: Return type: bool New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PredrillPointsUseEffectDist
Parameters: newValue (bool) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
RetractAreaBuilder¶
-
NcmPlanarBuilder.
RetractAreaBuilder
¶ Returns the retract area builder
-------------------------------------
Getter Method
Signature
RetractAreaBuilder
Returns: the retract area builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
RetractFinalBuilder¶
-
NcmPlanarBuilder.
RetractFinalBuilder
¶ Returns the final retract builder
-------------------------------------
Getter Method
Signature
RetractFinalBuilder
Returns: the final retract builder Return type: NXOpen.CAM.NcmPlanarEngRetBuilder
New in version NX5.0.0.
License requirements: None.
SmoothingBuilder¶
-
NcmPlanarBuilder.
SmoothingBuilder
¶ Returns the smoothing builder
-------------------------------------
Getter Method
Signature
SmoothingBuilder
Returns: The smoothing builder Return type: NXOpen.CAM.NcmSmoothingBuilder
New in version NX9.0.2.
License requirements: None.
SuppressCutcom¶
-
NcmPlanarBuilder.
SuppressCutcom
¶ Returns or sets the suppress cutter compensation
-------------------------------------
Getter Method
Signature
SuppressCutcom
Returns: Return type: bool New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SuppressCutcom
Parameters: suppressCutcom (bool) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
TransferAvoidanceFromBuilder¶
-
NcmPlanarBuilder.
TransferAvoidanceFromBuilder
¶ Returns the from point builder
-------------------------------------
Getter Method
Signature
TransferAvoidanceFromBuilder
Returns: The from point builder Return type: NXOpen.CAM.NcmAvoidancePointBuilder
New in version NX5.0.0.
License requirements: None.
TransferAvoidanceGohomeBuilder¶
-
NcmPlanarBuilder.
TransferAvoidanceGohomeBuilder
¶ Returns the gohome point builder
-------------------------------------
Getter Method
Signature
TransferAvoidanceGohomeBuilder
Returns: The gohome point builder Return type: NXOpen.CAM.NcmAvoidancePointBuilder
New in version NX5.0.0.
License requirements: None.
TransferAvoidanceReturnBuilder¶
-
NcmPlanarBuilder.
TransferAvoidanceReturnBuilder
¶ Returns the return point builder
-------------------------------------
Getter Method
Signature
TransferAvoidanceReturnBuilder
Returns: The return point builder Return type: NXOpen.CAM.NcmAvoidancePointBuilder
New in version NX5.0.0.
License requirements: None.
TransferAvoidanceStartBuilder¶
-
NcmPlanarBuilder.
TransferAvoidanceStartBuilder
¶ Returns the start point builder
-------------------------------------
Getter Method
Signature
TransferAvoidanceStartBuilder
Returns: The start point builder Return type: NXOpen.CAM.NcmAvoidancePointBuilder
New in version NX5.0.0.
License requirements: None.
TransferBetweenLevelsSafeDistanceBuilder¶
-
NcmPlanarBuilder.
TransferBetweenLevelsSafeDistanceBuilder
¶ Returns the transfer between levels safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
TransferBetweenLevelsSafeDistanceBuilder
Returns: The transfer between levels safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
TransferBetweenLevelsType¶
-
NcmPlanarBuilder.
TransferBetweenLevelsType
¶ Returns or sets the transfer between levels type
-------------------------------------
Getter Method
Signature
TransferBetweenLevelsType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderTransferBetweenLevelsTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransferBetweenLevelsType
Parameters: transferType ( NXOpen.CAM.NcmPlanarBuilderTransferBetweenLevelsTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TransferBetweenRegionsBuilder¶
-
NcmPlanarBuilder.
TransferBetweenRegionsBuilder
¶ Returns the Transfer Between Regions builder
-------------------------------------
Getter Method
Signature
TransferBetweenRegionsBuilder
Returns: Transfer Between Regions Return type: NXOpen.CAM.NcmTransfer
New in version NX9.0.0.
License requirements: None.
TransferBetweenRegionsSafeDistanceBuilder¶
-
NcmPlanarBuilder.
TransferBetweenRegionsSafeDistanceBuilder
¶ Returns the transfer between regions safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
TransferBetweenRegionsSafeDistanceBuilder
Returns: The transfer between regions safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.CAM.NcmTransfer.SafeDistanceBuilder()
instead.License requirements: None.
TransferBetweenRegionsType¶
-
NcmPlanarBuilder.
TransferBetweenRegionsType
¶ Returns or sets the transfer between regions type
-------------------------------------
Getter Method
Signature
TransferBetweenRegionsType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderTransferBetweenRegionsTypes
New in version NX5.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.CAM.NcmTransfer.Type()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
TransferBetweenRegionsType
Parameters: transferType ( NXOpen.CAM.NcmPlanarBuilderTransferBetweenRegionsTypes
) –New in version NX5.0.0.
Deprecated since version NX9.0.0: Please use
NXOpen.CAM.NcmTransfer.Type()
instead.License requirements: cam_base (“CAM BASE”)
TransferWithinLevelsHeightBuilder¶
-
NcmPlanarBuilder.
TransferWithinLevelsHeightBuilder
¶ Returns the transfer within levels height builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
TransferWithinLevelsHeightBuilder
Returns: The transfer within levels height builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
TransferWithinLevelsMaxFollowDistanceBuilder¶
-
NcmPlanarBuilder.
TransferWithinLevelsMaxFollowDistanceBuilder
¶ Returns the transfer within levels max follow distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
TransferWithinLevelsMaxFollowDistanceBuilder
Returns: The transfer within levels max follow distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
TransferWithinLevelsSafeDistanceBuilder¶
-
NcmPlanarBuilder.
TransferWithinLevelsSafeDistanceBuilder
¶ Returns the transfer within levels safe distance builder (inheritable tool dep)
-------------------------------------
Getter Method
Signature
TransferWithinLevelsSafeDistanceBuilder
Returns: The transfer within levels safe distance builder Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX5.0.0.
License requirements: None.
TransferWithinLevelsType¶
-
NcmPlanarBuilder.
TransferWithinLevelsType
¶ Returns or sets the transfer within levels type
-------------------------------------
Getter Method
Signature
TransferWithinLevelsType
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransferWithinLevelsType
Parameters: transferType ( NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
TransferWithinLevelsWith¶
-
NcmPlanarBuilder.
TransferWithinLevelsWith
¶ Returns or sets the transfer within levels strategy
-------------------------------------
Getter Method
Signature
TransferWithinLevelsWith
Returns: Return type: NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsWiths
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TransferWithinLevelsWith
Parameters: newValue ( NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsWiths
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetPredrillPoints¶
-
NcmPlanarBuilder.
GetPredrillPoints
¶ The pre-drill points
Signature
GetPredrillPoints()
Returns: Array of points Return type: list of NXOpen.Point
New in version NX5.0.0.
License requirements: None.
SetPredrillPoints¶
-
NcmPlanarBuilder.
SetPredrillPoints
¶ The pre-drill points
Signature
SetPredrillPoints(predrillPoints)
Parameters: predrillPoints (list of NXOpen.Point
) – Array of pointsNew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
NcmPlanarBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.