NcmPlanarBuilderFinalTypes Enumeration¶
NXOpen.CAM.NcmPlanarBuilder.FinalTypes is an alias for NXOpen.CAM.NcmPlanarBuilderFinalTypes
-
class
NXOpen.CAM.
NcmPlanarBuilderFinalTypes
¶ Bases:
object
Available types for final clearance in planar milling
Enum Members
Enum Member Enum Member Description Clearance tool axis clearance Distance distance NotSet none ShortestDistanceToClearance shortest distance to clearance CutPlaneToClearance cut plane to clearance -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-