BaseBuilder Class¶
-
class
NXOpen.CAM.
BaseBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.CAM.BaseBuilder
New in version NX11.0.1.
Methods¶
Method | Description |
---|---|
GetCustomizableItemBuilder | Returns the customizable item builder for given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetCustomizableItemBuilder¶
-
BaseBuilder.
GetCustomizableItemBuilder
¶ Returns the customizable item builder for given customizable item name
Signature
GetCustomizableItemBuilder(name)
Parameters: name (str) – CI name Returns: Return type: NXOpen.TaggedObject
New in version NX11.0.1.
License requirements: None.
GetCustomizableItemNames¶
-
BaseBuilder.
GetCustomizableItemNames
¶ Returns the names for all customizable item ids
Signature
GetCustomizableItemNames()
Returns: the ci names Return type: list of str New in version NX11.0.1.
License requirements: None.
Validate¶
-
BaseBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.