NcmPlanarBuilderTransferWithinLevelsTypes Enumeration¶
NXOpen.CAM.NcmPlanarBuilder.TransferWithinLevelsTypes is an alias for NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsTypes
-
class
NXOpen.CAM.
NcmPlanarBuilderTransferWithinLevelsTypes
¶ Bases:
object
Available types for transfer within levels in planar milling
Enum Members
Enum Member Enum Member Description LowestSafeZ lowest Safe Z PrevPlane previous plane Direct direct Clearance tool axis to clearance BlankPlane Blank Plane ShortestToClearance shortest to clearance CutPlaneToClearance cut plane to clearance Smooth smooth DirectPreviousPlaneBackup direct/previous plane backup CutPlane cut plane -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-