NcmPlanarBuilderTransferWithinLevelsWiths Enumeration¶
NXOpen.CAM.NcmPlanarBuilder.TransferWithinLevelsWiths is an alias for NXOpen.CAM.NcmPlanarBuilderTransferWithinLevelsWiths
-
class
NXOpen.CAM.
NcmPlanarBuilderTransferWithinLevelsWiths
¶ Bases:
object
Available strategies for transfer within levels in planar milling
Enum Members
Enum Member Enum Member Description UseEngret Use engage and retract defs FollowBoundary follow boundary (for future use) LiftPlunge lift and plunge NotSet none Smooth smooth -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-