ResultManager Class¶
-
class
NXOpen.CAE.
ResultManager
¶ Bases:
object
Manages results
To obtain an instance of this class, refer to
NXOpen.Session
New in version NX6.0.2.
Methods¶
Method | Description |
---|---|
ConstructSubmodelForResultAccessReferenceField | Creates a result access reference field object that is evaluated at node, element, or element-node id’s. |
ConvertOdbFile | Convert older version of ODB file to currently supported version |
Create3dGraphBuilder | Returns a builder used for creating 3d graphs across iterations. |
Create4dResultAccessReferenceField | Creates a result access reference field object that supports 4D (hetergeneous) domains such as time-cartesian. |
Create4dResultAccessReferenceFieldWithLimits | Creates a result access reference field object that supports 4D (hetergeneous) domains such as time-cartesian. |
CreateAxiSymmetricParameters | Creates a axisymmetric object based on an existing Post View It is user’s responsibility to destroy the result access object once done using NXOpen.CAE.ResultManager.DeleteAxiSymmetricParameters() , in order to free up system resources |
CreateClippingParameters | Creates a clipping parameter object. |
CreateCrossSectionParameters | Creates a cross section parameter object. |
CreateCyclicSymmetricParameters | Creates a cyclic symmetric object based on an existing Post View It is user’s responsibility to destroy the result access object once done using NXOpen.CAE.ResultManager.DeleteCyclicSymmetricParameters() , in order to free up system resources |
CreateDaoOptimizationSolutionResult | Creates a solution result object given a NXOpen.CAE.Optimization.DAOSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateDeformationParameters | Creates a deformation parameter object. |
CreateDurabilityEventResult | Creates a solution result object given a NXOpen.CAE.DurabilityEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateFreeBodyResultsBuilder | Creates a free body results builder. |
CreateGraphAcrossIterationsBuilder | Returns a builder used for creating graphs of Postview result values across iterations. |
CreateGraphAlongPathBuilder | Returns a builder used for creating the graph of result values of Postview result defined by series of entities or path object. |
CreateGraphFromResultProbesBuilder | Returns a builder used for creating graph from result probes. |
CreateGraphOrbitBuilder | Returns a builder used for creating the orbit graph from postview. |
CreateIdResultAccessReferenceField | Creates a result access reference field object that is evaluated at node, element, or element-node id’s. |
CreateImportedResult | Creates a imported result object given a solver results file and the unit systems that these results are defined in. |
CreateJtBuilder | Creates a builder for exporting a component or result type JT |
CreateLaminateDynamicEventResult | Creates a solution result object given a NXOpen.CAE.LaminateDynamicEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateLaminateGraphicalReportResult | Creates a solution result object given a NXOpen.CAE.LaminateGraphicalReport It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreatePostJtBuilder | Creates a builder for exporting a component or result type JT |
CreatePostSelectionEntity | Creates a selection entity object. |
CreateQueryCurvePost | Creates query curve from an ordered set |
CreateReferenceResult | Creates a reference result object given a NXOpen.CAE.SimResultReference It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateResponseEventResult | Creates a solution result object given a NXOpen.CAE.ResponseSimulation.RSEvent It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateResponseSolutionResult | Creates a solution result object given a NXOpen.CAE.ResponseSimulation.Solution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateResultAccess | Creates a result access object It is user’s responsibility to destroy the result access object once done using NXOpen.CAE.ResultManager.DeleteResultAccess() , in order to free up system resources |
CreateResultAccessReferenceField | Creates a result access reference field object. |
CreateResultParameters | Creates a result parameter object. |
CreateResultParametersWithNodalForceReport | Creates a result parameter object for given Free Body. |
CreateResultParametersWithProbe | Creates a result parameter object for given Result Probe. |
CreateResultsCombinationBuilder | Creates a results combination builder. |
CreateResultsEnvelopeBuilder | Creates a results envelope builder. |
CreateResultsModelExportBuilder | Creates a model export builder. |
CreateResultsReductionBuilder | Creates a results reduction builder. |
CreateResultvariable | Creates Result Variable object |
CreateSeResult | Creates a result object given a Super Element ID within an existing NXOpen.CAE.Result . |
CreateSolutionResult | Creates a solution result object given a NXOpen.CAE.SimSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateTableFieldForModel | Creates a table for the model. |
CreateTableFieldFromNodalForceReport | Creates a field from the lists of independent, dependent variables along with a given NodalForceReport. |
CreateTableFieldFromProbe | Creates a field from the lists of independent, dependent variables along with a given Result Probe. |
CreateTableOfFieldsForModel | Creates a table of fields for the model. |
CreateTbsOptimizationSolutionResult | Creates a solution result object given a NXOpen.CAE.Optimization.TBSOptimizationSolution It is user’s responsibility to destroy the result object once done using NXOpen.CAE.ResultManager.DeleteResult() , in order to free up system resources. |
CreateTransientResultsReductionBuilder | Creates a transient results reduction builder. |
DeleteAxiSymmetricParameters | Delete a NXOpen.CAE.AxiSymmetricParameters object. |
DeleteClippingParameters | Delete a NXOpen.CAE.ClippingParameters object. |
DeleteCrossSectionParameters | Delete a NXOpen.CAE.CrossSectionParameters object. |
DeleteCyclicSymmetricParameters | Delete a NXOpen.CAE.CyclicSymmetricParameters object. |
DeleteDeformationParameters | Delete a NXOpen.CAE.DeformationParameters object. |
DeleteFreeBodyResultsBuilder | Delete a NXOpen.CAE.FreeBodyResultsBuilder object. |
DeletePostJtBuilder | Delete a NXOpen.CAE.PostJtExportBuilder object. |
DeleteQueryCurve | Delete a QueryCurvePost |
DeleteResult | Delete a NXOpen.CAE.Result object. |
DeleteResultAccess | Delete a NXOpen.CAE.ResultAccess object. |
DeleteResultParameters | Delete a NXOpen.CAE.ResultParameters object. |
DeleteResultParametersWithNodalForceReport | Delete a NXOpen.CAE.ResultParametersWithNodalForceReport object. |
DeleteResultParametersWithProbe | Delete a NXOpen.CAE.ResultParametersWithProbe object. |
ExportUnvFromProbe | Exports Results from ResultProbe in UNV file format. |
FindObject | Returns a NXOpen.CAE.Result |
GetIterationsWithLimits | Get available iterations given the limits. |
OpenImportedResult | Opens a imported result object given a solver results file and the unit systems that these results are defined in. |
Method Detail¶
ConstructSubmodelForResultAccessReferenceField¶
-
ResultManager.
ConstructSubmodelForResultAccessReferenceField
¶ Creates a result access reference field object that is evaluated at node, element, or element-node id’s.
The created field is automatically made persistent and stored in the collection of fields for the part. A sub modle is used to filter the elem/nodes that need to be evaluated
Signature
ConstructSubmodelForResultAccessReferenceField(refField, fieldManager, result, elem, includeOrExculde)
Parameters: - refField (
NXOpen.Fields.FieldReference
) – field that in part - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - elem (list of int) – submodel element ID
- includeOrExculde (bool) –
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- refField (
ConvertOdbFile¶
-
ResultManager.
ConvertOdbFile
¶ Convert older version of ODB file to currently supported version
Signature
ConvertOdbFile(inputFileName, outputFileName)
Parameters: - inputFileName (str) –
- outputFileName (str) –
New in version NX6.0.2.
License requirements: None.
Create3dGraphBuilder¶
-
ResultManager.
Create3dGraphBuilder
¶ Returns a builder used for creating 3d graphs across iterations.
It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
Create3dGraphBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.Post3DGraphBuilder
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.CAE.ResultManager.CreateGraphFromResultProbesBuilder()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Create4dResultAccessReferenceField¶
-
ResultManager.
Create4dResultAccessReferenceField
¶ Creates a result access reference field object that supports 4D (hetergeneous) domains such as time-cartesian.
The created field is automatically made persistent and stored in the collection of fields for the part.
Signature
Create4dResultAccessReferenceField(fieldManager, result, parameters, indepDomainName, depDomainName, fieldName)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - indepDomainName (str) – alphanumeric string; it must match with existing domain names
- depDomainName (str) – alphanumeric string; it must match with existing domain names
- fieldName (str) – field name
Returns: Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- fieldManager (
Create4dResultAccessReferenceFieldWithLimits¶
-
ResultManager.
Create4dResultAccessReferenceFieldWithLimits
¶ Creates a result access reference field object that supports 4D (hetergeneous) domains such as time-cartesian.
The created field is automatically made persistent and stored in the collection of fields for the part. The primary independent domain is limited by the input
Signature
Create4dResultAccessReferenceFieldWithLimits(fieldManager, result, parameters, indepDomainName, depDomainName, fieldName, minLimit, maxLimit)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - indepDomainName (str) – alphanumeric string; it must match with existing domain names
- depDomainName (str) – alphanumeric string; it must match with existing domain names
- fieldName (str) – field name
- minLimit (list of int) – minimum loadcase,iteration and subiteration
- maxLimit (list of int) – maximum load case,iteration and subiteration
Returns: Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- fieldManager (
CreateAxiSymmetricParameters¶
-
ResultManager.
CreateAxiSymmetricParameters
¶ Creates a axisymmetric object based on an existing Post View It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteAxiSymmetricParameters()
, in order to free up system resourcesSignature
CreateAxiSymmetricParameters()
Returns: Return type: NXOpen.CAE.AxiSymmetricParameters
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateClippingParameters¶
-
ResultManager.
CreateClippingParameters
¶ Creates a clipping parameter object.
It is user’s responsibility to destroy the clipping parameters object once done using
NXOpen.CAE.ResultManager.DeleteClippingParameters()
, in order to free up system resourcesSignature
CreateClippingParameters()
Returns: Return type: NXOpen.CAE.ClippingParameters
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateCrossSectionParameters¶
-
ResultManager.
CreateCrossSectionParameters
¶ Creates a cross section parameter object.
It is user’s responsibility to destroy the cross section parameters object once done using
NXOpen.CAE.ResultManager.DeleteCrossSectionParameters()
, in order to free up system resourcesSignature
CreateCrossSectionParameters()
Returns: Return type: NXOpen.CAE.CrossSectionParameters
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateCyclicSymmetricParameters¶
-
ResultManager.
CreateCyclicSymmetricParameters
¶ Creates a cyclic symmetric object based on an existing Post View It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteCyclicSymmetricParameters()
, in order to free up system resourcesSignature
CreateCyclicSymmetricParameters()
Returns: Return type: NXOpen.CAE.CyclicSymmetricParameters
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateDaoOptimizationSolutionResult¶
-
ResultManager.
CreateDaoOptimizationSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.Optimization.DAOSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateDaoOptimizationSolutionResult(daoOptimizationSolution)
Parameters: daoOptimizationSolution ( NXOpen.CAE.Optimization.DAOSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateDeformationParameters¶
-
ResultManager.
CreateDeformationParameters
¶ Creates a deformation parameter object.
It is user’s responsibility to destroy the deformation parameters object once done using
NXOpen.CAE.ResultManager.DeleteDeformationParameters()
, in order to free up system resourcesSignature
CreateDeformationParameters()
Returns: Return type: NXOpen.CAE.DeformationParameters
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateDurabilityEventResult¶
-
ResultManager.
CreateDurabilityEventResult
¶ Creates a solution result object given a
NXOpen.CAE.DurabilityEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateDurabilityEventResult(durablityEvent)
Parameters: durablityEvent ( NXOpen.CAE.DurabilityEvent
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateFreeBodyResultsBuilder¶
-
ResultManager.
CreateFreeBodyResultsBuilder
¶ Creates a free body results builder.
It is user’s responsibility to destroy the builder object once done using
NXOpen.CAE.ResultManager.DeleteFreeBodyResultsBuilder()
, in order to free up system resourcesSignature
CreateFreeBodyResultsBuilder()
Returns: Return type: NXOpen.CAE.FreeBodyResultsBuilder
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateGraphAcrossIterationsBuilder¶
-
ResultManager.
CreateGraphAcrossIterationsBuilder
¶ Overloaded method CreateGraphAcrossIterationsBuilder
CreateGraphAcrossIterationsBuilder(pvid)
CreateGraphAcrossIterationsBuilder(firstpvid, secondpvid)
CreateGraphAcrossIterationsBuilder(result, parameter)
CreateGraphAcrossIterationsBuilder(parameter)
CreateGraphAcrossIterationsBuilder(result, parameter1, parameter2)
CreateGraphAcrossIterationsBuilder(result, parameters, names, formula)
-------------------------------------
Returns a builder used for creating graphs of Postview result values across iterations. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphAcrossIterationsBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating graphs of two postview result values across iterations. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(firstpvid, secondpvid)
Parameters: - firstpvid (int) –
- secondpvid (int) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.PostGraphAcrossIterationsBuilder
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.CAE.ResultManager.CreateGraphFromResultProbesBuilder()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values two result parameters. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameter1, parameter2)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter1 (
NXOpen.CAE.ResultParameters
) – - parameter2 (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating graphs across iterations of result values of expression. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAcrossIterationsBuilder(result, parameters, names, formula)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameters (list of
NXOpen.CAE.ResultParameters
) – set result parameters - names (list of str) – set result names
- formula (str) – set formula
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateGraphAlongPathBuilder¶
-
ResultManager.
CreateGraphAlongPathBuilder
¶ Overloaded method CreateGraphAlongPathBuilder
CreateGraphAlongPathBuilder(pvid)
CreateGraphAlongPathBuilder(firstpvid, secondpvid)
CreateGraphAlongPathBuilder(result, parameter)
CreateGraphAlongPathBuilder(parameter)
CreateGraphAlongPathBuilder(result, parameter1, parameter2)
-------------------------------------
Returns a builder used for creating the graph of result values of Postview result defined by series of entities or path object. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphAlongPathBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating the graph of result values of two postviews defined by series of entities or path object. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(firstpvid, secondpvid)
Parameters: - firstpvid (int) –
- secondpvid (int) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating the graph of result values series of entities or path object defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating the graph of result values series of entities or path object defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(parameter)
Parameters: parameter ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.PostGraphAlongPathBuilder
New in version NX10.0.0.
Deprecated since version NX11.0.0: Use
NXOpen.CAE.ResultManager.CreateGraphFromResultProbesBuilder()
instead.License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
-------------------------------------
Returns a builder used for creating the graph of result values of series of entities or path object defined by two result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphAlongPathBuilder(result, parameter1, parameter2)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter1 (
NXOpen.CAE.ResultParameters
) – - parameter2 (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateGraphFromResultProbesBuilder¶
-
ResultManager.
CreateGraphFromResultProbesBuilder
¶ Returns a builder used for creating graph from result probes.
It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphFromResultProbesBuilder()
Returns: Return type: NXOpen.CAE.GraphFromResultProbeBuilder
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateGraphOrbitBuilder¶
-
ResultManager.
CreateGraphOrbitBuilder
¶ Overloaded method CreateGraphOrbitBuilder
CreateGraphOrbitBuilder(pvid)
CreateGraphOrbitBuilder(result, parameter)
-------------------------------------
Returns a builder used for creating the orbit graph from postview. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphOrbitBuilder(pvid)
Parameters: pvid (int) – Returns: Return type: NXOpen.CAE.PostGraphOrbitBuilder
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Returns a builder used for creating the orbit graph from result defined by result parameter. It is user’s responsibility to destroy the builder object once done using
Builder.Destroy()
, in order to free up system resourcesSignature
CreateGraphOrbitBuilder(result, parameter)
Parameters: - result (
NXOpen.CAE.Result
) – set result - parameter (
NXOpen.CAE.ResultParameters
) –
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateIdResultAccessReferenceField¶
-
ResultManager.
CreateIdResultAccessReferenceField
¶ Creates a result access reference field object that is evaluated at node, element, or element-node id’s.
The created field is automatically made persistent and stored in the collection of fields for the part.
Signature
CreateIdResultAccessReferenceField(fieldManager, result, parameters, depDomainName, fieldName)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - depDomainName (str) – alphanumeric string; it must match with existing domain names
- fieldName (str) – field name
Returns: Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- fieldManager (
CreateImportedResult¶
-
ResultManager.
CreateImportedResult
¶ Overloaded method CreateImportedResult
CreateImportedResult(filename, unitsystem)
CreateImportedResult(filename, resultname, unitsystem)
CreateImportedResult(filename, resultname)
-------------------------------------
Creates a imported result object given a solver results file and the unit systems that these results are defined in. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resourcesSignature
CreateImportedResult(filename, unitsystem)
Parameters: - filename (str) –
- unitsystem (
NXOpen.CAE.ResultResultBasicUnit_Struct
) –
Returns: Return type: New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Creates a imported result object given a solver results file and the unit systems that these results are defined in. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resourcesSignature
CreateImportedResult(filename, resultname, unitsystem)
Parameters: - filename (str) –
- resultname (str) –
- unitsystem (
NXOpen.CAE.ResultResultBasicUnit_Struct
) –
Returns: Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Creates a imported result object given a solver results file. The unit systems is inferred from the result file and Part. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resourcesSignature
CreateImportedResult(filename, resultname)
Parameters: - filename (str) –
- resultname (str) –
Returns: Return type: New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateJtBuilder¶
-
ResultManager.
CreateJtBuilder
¶ Creates a builder for exporting a component or result type JT
Signature
CreateJtBuilder()
Returns: Return type: NXOpen.CAE.CreateJtBuilder
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateLaminateDynamicEventResult¶
-
ResultManager.
CreateLaminateDynamicEventResult
¶ Creates a solution result object given a
NXOpen.CAE.LaminateDynamicEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateLaminateDynamicEventResult(dynEvent)
Parameters: dynEvent ( NXOpen.CAE.LaminateDynamicEvent
) – The dynamic eventReturns: Created solution result given the input dynamic event Return type: NXOpen.CAE.SolutionResult
New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateLaminateGraphicalReportResult¶
-
ResultManager.
CreateLaminateGraphicalReportResult
¶ Creates a solution result object given a
NXOpen.CAE.LaminateGraphicalReport
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateLaminateGraphicalReportResult(lamGraphReport)
Parameters: lamGraphReport ( NXOpen.CAE.LaminateGraphicalReport
) – The laminate graphical report specificationsReturns: Created solution result given the input laminate graphical report specifications Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreatePostJtBuilder¶
-
ResultManager.
CreatePostJtBuilder
¶ Creates a builder for exporting a component or result type JT
Signature
CreatePostJtBuilder()
Returns: Return type: NXOpen.CAE.PostJtExportBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreatePostSelectionEntity¶
-
ResultManager.
CreatePostSelectionEntity
¶ Creates a selection entity object.
It is user’s responsibility to destroy the selection entity object once done using
NXOpen.CAE.PostSelectionEntity.Delete()
, in order to free up system resourcesSignature
CreatePostSelectionEntity()
Returns: Return type: NXOpen.CAE.PostSelectionEntity
New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateQueryCurvePost¶
-
ResultManager.
CreateQueryCurvePost
¶ Creates query curve from an ordered set
Signature
CreateQueryCurvePost(result, name, entities, numInsertPointsPerSegment)
Parameters: - result (
NXOpen.CAE.Result
) – Result - name (str) – Name of the post query curve
- entities (list of
NXOpen.CAE.QueryCurvePostEntity_Struct
) – Query curve entities array - numInsertPointsPerSegment (int) – Insert points between two consecuting entities
Returns: Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- result (
CreateReferenceResult¶
-
ResultManager.
CreateReferenceResult
¶ Creates a reference result object given a
NXOpen.CAE.SimResultReference
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateReferenceResult(solution)
Parameters: solution ( NXOpen.CAE.SimResultReference
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResponseEventResult¶
-
ResultManager.
CreateResponseEventResult
¶ Creates a solution result object given a
NXOpen.CAE.ResponseSimulation.RSEvent
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateResponseEventResult(responseSolution)
Parameters: responseSolution ( NXOpen.CAE.ResponseSimulation.RSEvent
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResponseSolutionResult¶
-
ResultManager.
CreateResponseSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.ResponseSimulation.Solution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateResponseSolutionResult(responseSolution)
Parameters: responseSolution ( NXOpen.CAE.ResponseSimulation.Solution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultAccess¶
-
ResultManager.
CreateResultAccess
¶ Overloaded method CreateResultAccess
CreateResultAccess(result, parameters)
CreateResultAccess(postViewID)
-------------------------------------
Creates a result access object It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteResultAccess()
, in order to free up system resourcesSignature
CreateResultAccess(result, parameters)
Parameters: - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access
Returns: Return type: New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Creates a result access object based on an existing Post View It is user’s responsibility to destroy the result access object once done using
NXOpen.CAE.ResultManager.DeleteResultAccess()
, in order to free up system resourcesSignature
CreateResultAccess(postViewID)
Parameters: postViewID (int) – an existing PostView Id Returns: Return type: NXOpen.CAE.ResultAccess
New in version NX8.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateResultAccessReferenceField¶
-
ResultManager.
CreateResultAccessReferenceField
¶ Overloaded method CreateResultAccessReferenceField
CreateResultAccessReferenceField(fieldManager, result, parameters, depDomainName, fieldName)
CreateResultAccessReferenceField(fieldManager, result, parameters, indepDomainName, depDomainName, fieldName)
-------------------------------------
Creates a result access reference field object. The created field is automatically made persistent and stored in the collection of fields for the part.
Signature
CreateResultAccessReferenceField(fieldManager, result, parameters, depDomainName, fieldName)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - depDomainName (str) – alphanumeric string; it must match with existing domain names
- fieldName (str) – field name
Returns: Return type: New in version NX9.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
Creates a result access reference field object with the specified independent domain. The created field is automatically made persistent and stored in the collection of fields for the part.
Signature
CreateResultAccessReferenceField(fieldManager, result, parameters, indepDomainName, depDomainName, fieldName)
Parameters: - fieldManager (
NXOpen.Fields.FieldManager
) – field manager in part - result (
NXOpen.CAE.Result
) – analysis results for which you want to access information - parameters (
NXOpen.CAE.ResultParameters
) – defines the specific results state you wish to access - indepDomainName (str) – alphanumeric string; it must match with existing domain names
- depDomainName (str) – alphanumeric string; it must match with existing domain names
- fieldName (str) – field name
Returns: Return type: New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
-------------------------------------
CreateResultParameters¶
-
ResultManager.
CreateResultParameters
¶ Creates a result parameter object.
It is user’s responsibility to destroy the result parameters object once done using
NXOpen.CAE.ResultManager.DeleteResultParameters()
, in order to free up system resourcesSignature
CreateResultParameters()
Returns: Return type: NXOpen.CAE.ResultParameters
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultParametersWithNodalForceReport¶
-
ResultManager.
CreateResultParametersWithNodalForceReport
¶ Creates a result parameter object for given Free Body.
It is user’s responsibility to destroy the result parameters object once done using
NXOpen.CAE.ResultManager.DeleteResultParametersWithNodalForceReport()
, in order to free up system resourcesSignature
CreateResultParametersWithNodalForceReport(nodalForceReport)
Parameters: nodalForceReport ( NXOpen.CAE.NodalForceReport
) –Returns: Return type: NXOpen.CAE.ResultParametersWithNodalForceReport
New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultParametersWithProbe¶
-
ResultManager.
CreateResultParametersWithProbe
¶ Creates a result parameter object for given Result Probe.
It is user’s responsibility to destroy the result parameters object once done using
NXOpen.CAE.ResultManager.DeleteResultParametersWithProbe()
, in order to free up system resourcesSignature
CreateResultParametersWithProbe(resultProbe)
Parameters: resultProbe ( NXOpen.CAE.ResultProbe
) –Returns: Return type: NXOpen.CAE.ResultParametersWithProbe
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateResultsCombinationBuilder¶
-
ResultManager.
CreateResultsCombinationBuilder
¶ Creates a results combination builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsCombinationBuilder()
Returns: Return type: NXOpen.CAE.ResultsCombinationBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultsEnvelopeBuilder¶
-
ResultManager.
CreateResultsEnvelopeBuilder
¶ Creates a results envelope builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsEnvelopeBuilder()
Returns: Return type: NXOpen.CAE.ResultsEnvelopeBuilder
New in version NX7.5.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultsModelExportBuilder¶
-
ResultManager.
CreateResultsModelExportBuilder
¶ Creates a model export builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsModelExportBuilder()
Returns: Return type: NXOpen.CAE.ResultsModelExportBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultsReductionBuilder¶
-
ResultManager.
CreateResultsReductionBuilder
¶ Creates a results reduction builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateResultsReductionBuilder()
Returns: Return type: NXOpen.CAE.ResultsReductionBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateResultvariable¶
-
ResultManager.
CreateResultvariable
¶ Creates Result Variable object
Signature
CreateResultvariable(sim, quan, loc, comp, restypename, name)
Parameters: - sim (
NXOpen.CAE.SimSimulation
) – Simulation - quan (
NXOpen.CAE.ResultQuantity
) – - loc (
NXOpen.CAE.ResultLocation
) – - comp (
NXOpen.CAE.ResultComponent
) – - restypename (str) – Result Type UserName, If not sure pass empty string
- name (str) – Result Variable name
Returns: Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- sim (
CreateSeResult¶
-
ResultManager.
CreateSeResult
¶ Creates a result object given a Super Element ID within an existing
NXOpen.CAE.Result
.It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resourcesSignature
CreateSeResult(parentResult, seid)
Parameters: - parentResult (
NXOpen.CAE.Result
) – - seid (int) –
Returns: Return type: New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
- parentResult (
CreateSolutionResult¶
-
ResultManager.
CreateSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.SimSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateSolutionResult(solution)
Parameters: solution ( NXOpen.CAE.SimSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateTableFieldForModel¶
-
ResultManager.
CreateTableFieldForModel
¶ Creates a table for the model.
A submodel could be used when creating the table.
Signature
CreateTableFieldForModel(fieldName, indepDomainType, depDomainType, nodevalshare, pvid, isdeform, elem, includeOrExculde)
Parameters: - fieldName (str) – field name
- indepDomainType (int) – Independe domain type, must not be heterogeneous domain
- depDomainType (int) – Dependent domain type, must not be heterogeneous domain
- nodevalshare (int) – Data manupulation type
- pvid (int) – Post view id
- isdeform (bool) – If the current view is deformed or not
- elem (list of int) – Submodel elements
- includeOrExculde (bool) – if the submodel elements are included or excluded
Returns: The table of fields created
Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateTableFieldFromNodalForceReport¶
-
ResultManager.
CreateTableFieldFromNodalForceReport
¶ Creates a field from the lists of independent, dependent variables along with a given NodalForceReport.
Signature
CreateTableFieldFromNodalForceReport(fieldName, indepVarArray, depVarArray, nodalForceReport)
Parameters: - fieldName (str) – field name
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the table field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables to be associated with the table field - nodalForceReport (
NXOpen.CAE.NodalForceReport
) –
Returns: field
Return type: New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateTableFieldFromProbe¶
-
ResultManager.
CreateTableFieldFromProbe
¶ Creates a field from the lists of independent, dependent variables along with a given Result Probe.
Signature
CreateTableFieldFromProbe(fieldName, indepVarArray, depVarArray, resultProbe, createTableOfFields)
Parameters: - fieldName (str) – field name
- indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the table field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables to be associated with the table field - resultProbe (
NXOpen.CAE.ResultProbe
) – - createTableOfFields (bool) – When output field is both time/frequency and space varying, it is possible to create a table of fields
Returns: field
Return type: New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CreateTableOfFieldsForModel¶
-
ResultManager.
CreateTableOfFieldsForModel
¶ Creates a table of fields for the model.
A submodel could be used when creating the table. A 4d field is created.
Signature
CreateTableOfFieldsForModel(fieldName, indepDomainType, depDomainType, nodevalshare, pvid, isdeform, elem, node, includeOrExculde, primValues, lcases, iters, subiters)
Parameters: - fieldName (str) – field name
- indepDomainType (int) – Independe domain type, must be heterogeneous domain
- depDomainType (int) – Dependent domain type, must not be heterogeneous domain
- nodevalshare (int) – Data manupulation type
- pvid (int) – Post view id
- isdeform (bool) – If the current view is deformed or not
- elem (list of int) – Submodel elements
- node (list of int) – Submodel nodes. Nodes are added primarily for elemental-nodal type of table, where not all nodes of a elements are in the table
- includeOrExculde (bool) – if the submodel are included or excluded
- primValues (list of float) – primary independent domain variable values
- lcases (list of int) – Load cases for the primary independent domain variable
- iters (list of int) – Iterations for the primary independent domain variable
- subiters (list of int) – Sub Iterations for the primary independent domain variable
Returns: The table of fields created
Return type: New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateTbsOptimizationSolutionResult¶
-
ResultManager.
CreateTbsOptimizationSolutionResult
¶ Creates a solution result object given a
NXOpen.CAE.Optimization.TBSOptimizationSolution
It is user’s responsibility to destroy the result object once done usingNXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resources.More than one
NXOpen.CAE.SolutionResult
object can be created for same solution, it is user’s responsibility to delete each one of them.Signature
CreateTbsOptimizationSolutionResult(tbsOptimizationSolution)
Parameters: tbsOptimizationSolution ( NXOpen.CAE.Optimization.TBSOptimizationSolution
) –Returns: Return type: NXOpen.CAE.SolutionResult
New in version NX8.0.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
CreateTransientResultsReductionBuilder¶
-
ResultManager.
CreateTransientResultsReductionBuilder
¶ Creates a transient results reduction builder.
It is user’s responsibility to destroy the builder object once done
Signature
CreateTransientResultsReductionBuilder()
Returns: Return type: NXOpen.CAE.TransientResultsReductionBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteAxiSymmetricParameters¶
-
ResultManager.
DeleteAxiSymmetricParameters
¶ Delete a
NXOpen.CAE.AxiSymmetricParameters
object.Signature
DeleteAxiSymmetricParameters(axiSymmetricParameter)
Parameters: axiSymmetricParameter ( NXOpen.CAE.AxiSymmetricParameters
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteClippingParameters¶
-
ResultManager.
DeleteClippingParameters
¶ Delete a
NXOpen.CAE.ClippingParameters
object.Signature
DeleteClippingParameters(result)
Parameters: result ( NXOpen.CAE.ClippingParameters
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteCrossSectionParameters¶
-
ResultManager.
DeleteCrossSectionParameters
¶ Delete a
NXOpen.CAE.CrossSectionParameters
object.Signature
DeleteCrossSectionParameters(crossSection)
Parameters: crossSection ( NXOpen.CAE.CrossSectionParameters
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteCyclicSymmetricParameters¶
-
ResultManager.
DeleteCyclicSymmetricParameters
¶ Delete a
NXOpen.CAE.CyclicSymmetricParameters
object.Signature
DeleteCyclicSymmetricParameters(cyclicSymmetricParameter)
Parameters: cyclicSymmetricParameter ( NXOpen.CAE.CyclicSymmetricParameters
) –New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteDeformationParameters¶
-
ResultManager.
DeleteDeformationParameters
¶ Delete a
NXOpen.CAE.DeformationParameters
object.Signature
DeleteDeformationParameters(result)
Parameters: result ( NXOpen.CAE.DeformationParameters
) –New in version NX7.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteFreeBodyResultsBuilder¶
-
ResultManager.
DeleteFreeBodyResultsBuilder
¶ Delete a
NXOpen.CAE.FreeBodyResultsBuilder
object.Signature
DeleteFreeBodyResultsBuilder(builder)
Parameters: builder ( NXOpen.CAE.FreeBodyResultsBuilder
) –New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeletePostJtBuilder¶
-
ResultManager.
DeletePostJtBuilder
¶ Delete a
NXOpen.CAE.PostJtExportBuilder
object.Signature
DeletePostJtBuilder(builder)
Parameters: builder ( NXOpen.CAE.PostJtExportBuilder
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteQueryCurve¶
-
ResultManager.
DeleteQueryCurve
¶ Delete a QueryCurvePost
Signature
DeleteQueryCurve(queryCurvePost)
Parameters: queryCurvePost ( NXOpen.CAE.QueryCurvePost
) – Query curve post to be deletedNew in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteResult¶
-
ResultManager.
DeleteResult
¶ Delete a
NXOpen.CAE.Result
object.If a
NXOpen.CAE.ResultAccess
object referencing it, that will also be deleted. This will only delete the the result passed to it and not other instances of Result Object.Signature
DeleteResult(result)
Parameters: result ( NXOpen.CAE.Result
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteResultAccess¶
-
ResultManager.
DeleteResultAccess
¶ Delete a
NXOpen.CAE.ResultAccess
object.Signature
DeleteResultAccess(result)
Parameters: result ( NXOpen.CAE.ResultAccess
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteResultParameters¶
-
ResultManager.
DeleteResultParameters
¶ Delete a
NXOpen.CAE.ResultParameters
object.Signature
DeleteResultParameters(result)
Parameters: result ( NXOpen.CAE.ResultParameters
) –New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
DeleteResultParametersWithNodalForceReport¶
-
ResultManager.
DeleteResultParametersWithNodalForceReport
¶ Delete a
NXOpen.CAE.ResultParametersWithNodalForceReport
object.Signature
DeleteResultParametersWithNodalForceReport(result)
Parameters: result ( NXOpen.CAE.ResultParametersWithNodalForceReport
) –New in version NX11.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DeleteResultParametersWithProbe¶
-
ResultManager.
DeleteResultParametersWithProbe
¶ Delete a
NXOpen.CAE.ResultParametersWithProbe
object.Signature
DeleteResultParametersWithProbe(result)
Parameters: result ( NXOpen.CAE.ResultParametersWithProbe
) –New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
ExportUnvFromProbe¶
-
ResultManager.
ExportUnvFromProbe
¶ Exports Results from ResultProbe in UNV file format.
Signature
ExportUnvFromProbe(fileName, probeArray)
Parameters: - fileName (str) – file name with full path
- probeArray (list of
NXOpen.CAE.ResultProbe
) – ResultProbes
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindObject¶
-
ResultManager.
FindObject
¶ Returns a
NXOpen.CAE.Result
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.TaggedObject
New in version NX7.5.1.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
GetIterationsWithLimits¶
-
ResultManager.
GetIterationsWithLimits
¶ Get available iterations given the limits.
numLimitItems must be 3 specifying that minLimit and maxLimit contains min/max 1.loadcase, 2. iteration and 3. subiteration
Signature
GetIterationsWithLimits(resid, lcase, iteration, superiter, minLimit, maxLimit)
Parameters: - resid (int) – result id
- lcase (int) – load case to look for
- iteration (int) – iteration to look for
- superiter (int) – super iteration to look for
- minLimit (list of int) – minimum loadcase,iteration and subiteration
- maxLimit (list of int) – maximum load case,iteration and subiteration
Returns: a tuple
Return type: A tuple consisting of (primValues, lcases, iters, subiters) primValues is a list of float. primary independent domain variable valueslcases is a list of int. Load cases for the primary independent domain variableiters is a list of int. Iterations for the primary independent domain variablesubiters is a list of int. Sub Iterations for the primary independent domain variable
New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”) OR sc_results_viewer (” Simcenter Results Viewer”)
OpenImportedResult¶
-
ResultManager.
OpenImportedResult
¶ Opens a imported result object given a solver results file and the unit systems that these results are defined in.
If there is no root part found then this api will open a part and then import the result in it. It is user’s responsibility to destroy the result object once done using
NXOpen.CAE.ResultManager.DeleteResult()
, in order to free up system resourcesSignature
OpenImportedResult(filename, resultname, unitsystem)
Parameters: - filename (str) –
- resultname (str) –
- unitsystem (
NXOpen.CAE.ResultResultBasicUnit_Struct
) –
Returns: Return type: New in version NX12.0.0.
License requirements: sc_results_viewer (” Simcenter Results Viewer”)