FieldLinksTable Class¶
-
class
NXOpen.Fields.
FieldLinksTable
¶ Bases:
NXOpen.Fields.Field
Represents the Field LinksTable class.
A field (see
NXOpen.Fields.Field
) defined in terms of tabular data involving one look-up independent column, an equal number of look-up fields and one or more dependent variables (seeNXOpen.Fields.FieldVariable
). This is similar to a table (seeNXOpen.Fields.FieldTable
), except instead of the interpolation dependent values being defined as numerical contants, they are defined by another field.To obtain a instance of this class use
NXOpen.Fields.FieldManager
.New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
Color | Returns or sets the color of the object. |
Discontinuities | Returns a flag specifying if the table has discontinuites |
IsBlanked | Returns the blank status of this object. |
IsLocked | Returns a value that indicates whether this field is locked against edits. |
IsOccurrence | Returns whether this object is an occurrence or not. |
IsUserField | Returns a value that indicates whether this field is a user created/managed field. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Layer | Returns or sets the layer that the object is in. |
LineFont | Returns or sets the line font of the object. |
LineWidth | Returns or sets the line width of the object. |
Name | Returns the custom name of the object. |
NameLocation | Returns the location of the object’s name. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
ValuesOutsideTableInterpolation | Returns or sets the outside table values interpolation method for linear interpolation |
Methods¶
Method | Description |
---|---|
AddApplicationData | Adds the specified application data object to the field NOTE: Only one application data object per IApplication can be added and the data must be owned by an IApplication with the same Part::Field::Main as the field. |
Blank | Blanks the object. |
CopyAsTableToPart | Create a new table field from this field (regardless of type). |
CopyToPart | Copy the field to the target part. |
CreateAttributeIterator | Create an attribute iterator |
CreateCopyInPart | Copy the field to the target part. |
CreateDrawHelper | Creates a field drawhelper which can be used to get display attributes of this field. |
CreateTableInPart | Create a new table field from this field (regardless of type). |
Delete | Delete this field; destroys the field and removes all references to it. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EditFieldLinksTable | Edit the LinksTable field. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetApplicationData | Retrieves the application data associated with the field for the specified application. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetDependentVariables | Returns the dependent variables for this NXOpen.Fields.Field |
GetDescription | Returns the description of the field. |
GetFieldDrawhelper | Returns a field drawhelper which can be used to get display attributes of this field. |
GetFieldEvaluator | Returns a field evaluator which can be used to evaluate this field. |
GetIdLabel | Returns the ID/Label of the field. |
GetIndependentVariables | Returns the independent variables for this NXOpen.Fields.Field |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSpatialMap | Returns the spatial map for the formula field if one exists. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Highlight | Highlights the object. |
Prints a representation of this object to the system log file. | |
RedisplayObject | Redisplays the object in all views. |
RemoveViewDependency | Remove dependency on all views from an object. |
Rename | Update the name of the field. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetDescription | Update the description of the field. |
SetIdLabel | Update the ID/Label of the field. |
SetName | Sets the custom name of the object. |
SetNameLocation | Sets the location of the object’s name. |
SetPartContext | Set part context. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetSecondaryValuesOutsideTableInterpolation | Set the values outside table interpolation option for sub fields if the sub fields are tables |
SetSpatialMap | Set the spatial map for the formula field. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Unblank | Unblanks the object. |
Unhighlight | Unhighlights the object. |
XYGraph | Creates displayed graphs of the Field’s specified independent variable versus all the Field’s dependent variables |
XYGraph3D | Plots or overlays graphs of the Field’s specified x-axis and z-axis independent variables versus the Field’s specified y-axis dependent variable ; returns newly created plot object. |
XYGraphArgand | Plots the Field’s specified independent variable versus all the Field’s scaled dependent variables as an Argand graph; returns newly created plot object(s). |
Property Detail¶
Discontinuities¶
-
FieldLinksTable.
Discontinuities
¶ Returns a flag specifying if the table has discontinuites
-------------------------------------
Getter Method
Signature
Discontinuities
Returns: a flag specifying if the links table or any referenced field tables has discontinuites Return type: bool New in version NX9.0.0.
License requirements: None.
IsOccurrence¶
-
FieldLinksTable.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
FieldLinksTable.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
FieldLinksTable.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
FieldLinksTable.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
FieldLinksTable.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
FieldLinksTable.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
ValuesOutsideTableInterpolation¶
-
FieldLinksTable.
ValuesOutsideTableInterpolation
¶ Returns or sets the outside table values interpolation method for linear interpolation
-------------------------------------
Getter Method
Signature
ValuesOutsideTableInterpolation
Returns: the outside table values interpolation method Return type: NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ValuesOutsideTableInterpolation
Parameters: interpolationMethod ( NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
) – the outside table values interpolation methodNew in version NX9.0.0.
License requirements: None.
Method Detail¶
EditFieldLinksTable¶
-
FieldLinksTable.
EditFieldLinksTable
¶ Overloaded method EditFieldLinksTable
EditFieldLinksTable(indepVarArray, depVarArray, datapoints, linkFieldsArray)
EditFieldLinksTable(indepVarArray, depVarArray, datapoints, linkFieldsArray, managedFieldsArray)
-------------------------------------
Edit the LinksTable field. Specifies the new array of :py:class:`NXOpen.Fields.FieldVariable`s for independent and dependent variables, as well as the new double values and linked fields. The datapoints and linked fields arrays are row based and number of each must equal the num_rows. The data_points array represents the values for the first independent value. For example, if the LinksTable has a domain of txyz, the values in this array are all values of t. The linked fields array must consist of the fields with independent variables representing the remaining variables in the independent domain of the LinksTable. For example, if the LinksTable has a domain of txyz, the independent domain of the fields in this array are all xyz. NULL values are allowed for linked fields and indicate a discontinuity at the associated value of the first independent variable. The dependent quantities are determined from the linked fields. The linked fields must have the same dependent variables as the Linkstable.
Signature
EditFieldLinksTable(indepVarArray, depVarArray, datapoints, linkFieldsArray)
Parameters: - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables of this and all linked fields - datapoints (list of float) – row based array of double values representing the first independent variable; the number of points should equal the number of rows.
- linkFieldsArray (list of
NXOpen.Fields.Field
) – row based array of link field values representing the table; the number of fields should equal the number of rows.
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Edit the LinksTable field. Specifies the new array of :py:class:`NXOpen.Fields.FieldVariable`s for independent and dependent variables, as well as the new double values and linked fields. The datapoints, linked fields, and the managed fields arrays are row based and number of each must equal the num_rows. The data_points array represents the values for the first independent value. For example, if the LinksTable has a domain of txyz, the values in this array are all values of t. The linked fields array must consist of the fields with independent variables representing the remaining variables in the independent domain of the LinksTable. For example, if the LinksTable has a domain of txyz, the independent domain of the fields in this array are all xyz. NULL values are allowed for linked fields and indicate a discontinuity at the associated value of the first independent variable. The dependent quantities are determined from the linked fields. The linked fields must have the same dependent variables as the Linkstable. The managed fields array identifies the fields that should be managed by the links table.
Signature
EditFieldLinksTable(indepVarArray, depVarArray, datapoints, linkFieldsArray, managedFieldsArray)
Parameters: - indepVarArray (list of
NXOpen.Fields.FieldVariable
) – independent variables to be associated with the field - depVarArray (list of
NXOpen.Fields.FieldVariable
) – dependent variables of this and all linked fields - datapoints (list of float) – row based array of double values representing the first independent variable; the number of points should equal the number of rows.
- linkFieldsArray (list of
NXOpen.Fields.Field
) – row based array of link field values representing the table; the number of fields should equal the number of rows. - managedFieldsArray (list of bool) – row based array of logical values indicating the links table field should manage the specified fields .
New in version NX9.0.0.
License requirements: None.
-------------------------------------
FindObject¶
-
FieldLinksTable.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
FieldLinksTable.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
FieldLinksTable.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetSecondaryValuesOutsideTableInterpolation¶
-
FieldLinksTable.
SetSecondaryValuesOutsideTableInterpolation
¶ Set the values outside table interpolation option for sub fields if the sub fields are tables
Signature
SetSecondaryValuesOutsideTableInterpolation(interpolationMethod)
Parameters: interpolationMethod ( NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
) – the outside table values interpolation method for sub fieldsNew in version NX12.0.0.
License requirements: None.