FieldEvaluatorValuesOutsideTableInterpolationEnum Enumeration¶
NXOpen.Fields.FieldEvaluator.ValuesOutsideTableInterpolationEnum is an alias for NXOpen.Fields.FieldEvaluatorValuesOutsideTableInterpolationEnum
-
class
NXOpen.Fields.
FieldEvaluatorValuesOutsideTableInterpolationEnum
¶ Bases:
object
Options for outside table values interpolation
Enum Members
Enum Member Enum Member Description Undefined No interpolation result Extrapolate Extrapolates from the boundary out into space using the same interpolation method that the interpolator for interior table values uses Constant Returns the boundary value as interpolation result Linear Extrapolates from the boundary out into space using the linear extrapolation method Parabolic Extrapolates from the boundary out into space using the parabolic extrapolation method Cubic Extrapolates from the boundary out into space using the cubic extrapolation method -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-