ResultsModelExportBuilder Class¶
-
class
NXOpen.CAE.
ResultsModelExportBuilder
¶ Bases:
NXOpen.CAE.ResultsManipulationBuilder
Represents a
NXOpen.CAE.ResultsModelExportBuilder
To obtain an instance of this class use
NXOpen.Session.ResultManager()
.New in version NX8.5.0.
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetAction | The action |
SetAppendMethod | The append method if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultName | The companion result name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionResultReference | The companion Result Reference if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCompanionSolution | The companion solution if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateCompanionResult |
SetCreateSolution | Specifies whether to create an imported solution |
SetImportResult | Import the result immediately |
SetImportedSolutionName | The imported solution name if action is NXOpen.CAE.ResultsManipulationBuilderAction.CreateImportedSolution |
SetIncludeModel | Include nodes and elements |
SetLoadcaseName | The load case name |
SetOutputFile | The output file |
SetOutputName | The output name |
SetOutputQuantity | The output quantity |
SetOutputResultType | The result output type |
SetResult | The result the model of which is to be exported |
SetUnitsSystem | The units system |
SetUnitsSystemResult | The result to copy the units system from |
SetUserDefinedUnitsSystem | The user-defined units system |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
SetResult¶
-
ResultsModelExportBuilder.
SetResult
¶ The result the model of which is to be exported
Signature
SetResult(result)
Parameters: result ( NXOpen.CAE.Result
) – set resultNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ResultsModelExportBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.