BaseFEModel Class¶
-
class
NXOpen.CAE.
BaseFEModel
¶ Bases:
NXOpen.CAE.IFEModel
This class represents an Assembly Finite Element Model. This class will act as the gateway to the Finite Element Nodes (
NXOpen.CAE.FENode
) and Elements (NXOpen.CAE.FEElement
) in the model. Only one instance of this class will exist in each assyfem part fileTo obtain an instance of this class, use
NXOpen.CAE.BaseFemPart.BaseFEModel()
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ConnectionsContainer | Returns the universal connection container. |
ConnectionsRootFolder | Returns the root connection folder. |
FeelementLabelMap | Returns a CAE.FEElement Label to CAE.FEElement Map for this Interface to the Finite Element Model. |
FenodeLabelMap | Returns a CAE.FENode Label to CAE.FENode Map for this Interface to the Finite Element Model. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
MeshManager | Returns the IMeshManager |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Tag | Returns the Tag for this object. |
BeamSections | Returns the Beam Section collection belonging to the part |
NodeElementMgr | Returns the node element manager belonging to this fem part |
CaeConnections | Returns the connection collector manager belonging to the part |
MeshControls | Returns the mesh control collection belonging to this fem part |
Bolts | Returns the connection collector manager belonging to the part |
FluidDomains | Returns the fluid domain collection belonging to this fem part |
CfdLocalResolutionConstraints | Returns the fluid domain local resolution constraint collection belonging to this fem part |
CfdContactPreventionConstraints | Returns the fluid domain contact prevention constraint collection belonging to this fem part |
CfdAutoRefinementConstraints | Returns the fluid domain automatic refinement constraint collection belonging to this fem part |
CaeReuseLibrary | Returns the CaeReuseLibrary belonging to the part |
ConnectionElementCollection | Return the NXOpen.CAE.Connections.Element collection of this object |
Methods¶
Method | Description |
---|---|
AskUpdatePending | This method will inform caller if the finite element model is in an update pending state or not. |
CreateAttributeIterator | Create an attribute iterator |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
EnableFemUpdate | This method will enable fem update. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetPdmReferenceAttributeValue | Gets the value of PDM Reference attribute for given object. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetName | Sets the custom name of the object. |
SetPdmReferenceAttribute | Sets the value of PDM Reference attribute on the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
UpdateFemodel | This method will update the finite element model so that it is in sync with any underlying changes. |
Property Detail¶
ConnectionsRootFolder¶
-
BaseFEModel.
ConnectionsRootFolder
¶ Returns the root connection folder.
-------------------------------------
Getter Method
Signature
ConnectionsRootFolder
Returns: the root folder holding all folder hierarchy and connections Return type: NXOpen.CAE.Connections.Folder
New in version NX11.0.0.
Deprecated since version NX12.0.0: For access to universal connections and folders use
CAE.IFEModel.ConnectionsContainer()
.License requirements: None.
IsOccurrence¶
-
BaseFEModel.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
BaseFEModel.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
BaseFEModel.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
BaseFEModel.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
BaseFEModel.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
BaseFEModel.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
BeamSections¶
-
BaseFEModel.
BeamSections
¶ Returns the Beam Section collection belonging to the part
Signature
BeamSections
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.BeamSectionCollection
NodeElementMgr¶
-
BaseFEModel.
NodeElementMgr
¶ Returns the node element manager belonging to this fem part
Signature
NodeElementMgr
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.NodeElementManager
CaeConnections¶
-
BaseFEModel.
CaeConnections
¶ Returns the connection collector manager belonging to the part
Signature
CaeConnections
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.CAEConnectionCollection
MeshControls¶
-
BaseFEModel.
MeshControls
¶ Returns the mesh control collection belonging to this fem part
Signature
MeshControls
New in version NX3.0.0.
Returns: Return type: NXOpen.CAE.MeshControlCollection
Bolts¶
-
BaseFEModel.
Bolts
¶ Returns the connection collector manager belonging to the part
Signature
Bolts
New in version NX7.5.0.
Returns: Return type: NXOpen.CAE.BoltCollection
FluidDomains¶
-
BaseFEModel.
FluidDomains
¶ Returns the fluid domain collection belonging to this fem part
Signature
FluidDomains
New in version NX7.5.2.
Returns: Return type: NXOpen.CAE.FluidDomainCollection
CfdLocalResolutionConstraints¶
-
BaseFEModel.
CfdLocalResolutionConstraints
¶ Returns the fluid domain local resolution constraint collection belonging to this fem part
Signature
CfdLocalResolutionConstraints
New in version NX9.0.0.
Returns: Return type: NXOpen.CAE.CfdLocalResolutionConstraintCollection
CfdContactPreventionConstraints¶
-
BaseFEModel.
CfdContactPreventionConstraints
¶ Returns the fluid domain contact prevention constraint collection belonging to this fem part
Signature
CfdContactPreventionConstraints
New in version NX9.0.0.
Returns: Return type: NXOpen.CAE.CfdContactPreventionConstraintCollection
CfdAutoRefinementConstraints¶
-
BaseFEModel.
CfdAutoRefinementConstraints
¶ Returns the fluid domain automatic refinement constraint collection belonging to this fem part
Signature
CfdAutoRefinementConstraints
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.CfdAutoRefinementConstraintCollection
CaeReuseLibrary¶
-
BaseFEModel.
CaeReuseLibrary
¶ Returns the CaeReuseLibrary belonging to the part
Signature
CaeReuseLibrary
New in version NX7.5.2.
Returns: Return type: NXOpen.Tooling.CaeReuseLibrary
ConnectionElementCollection¶
-
BaseFEModel.
ConnectionElementCollection
¶ Return the
NXOpen.CAE.Connections.Element
collection of this objectSignature
ConnectionElementCollection
New in version NX11.0.0.
Returns: Return type: NXOpen.CAE.Connections.ElementCollection
Method Detail¶
AskUpdatePending¶
-
BaseFEModel.
AskUpdatePending
¶ This method will inform caller if the finite element model is in an update pending state or not.
if update_pending is true, can call
NXOpen.CAE.BaseFEModel.UpdateFemodel()
to get model up-to-date.Signature
AskUpdatePending()
Returns: true if update is required Return type: bool New in version NX12.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
EnableFemUpdate¶
-
BaseFEModel.
EnableFemUpdate
¶ This method will enable fem update.
All the morphed meshes would be made orphan
Signature
EnableFemUpdate()
New in version NX10.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
FindObject¶
-
BaseFEModel.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Print¶
-
BaseFEModel.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
BaseFEModel.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
UpdateFemodel¶
-
BaseFEModel.
UpdateFemodel
¶ This method will update the finite element model so that it is in sync with any underlying changes.
All FE Meshes that are in the update pending state will be remeshed.
Signature
UpdateFemodel()
New in version NX6.0.2.
License requirements: nx_masterfem (“Finite Element Modeling”)